• Configure Baudrate ADUCM3029

    Hello.

    I want to set my baudrate to 9600 and I have found a function description to set baudrate by configuring the fractional divisors found below. It provide an equation to calculate the baudrate but I'm not yet familiar with the parameters what would…

  • ADUCM3029 cstack location

    I m working with ADUCM3029 under the MODE3 ram configuration . And the Cstack is placed at end of dRAM_always_retained_region by default.I want to move it to the end of dRAM_bank2_retained_region. When i did so, i can build the project, but when i start…

  • Transmit data to serial emulator with UART ADUCM3029

    Hello.

    I have code snippet below that uses ADC to sample the input signal at channel 0 and write the acquired samples to a serial emulator(Realterm). It uses UART device driver for autobaud rate detection that is it waits to transmit the samples to serial…

  • ADuCM3029 DC Offset

    Hello,

    I am using the ADuCM3029. 

    While in both the low and high frequency loops, 

    When I produce a DAC sinusoid output signal, there seems to be a DC offset in the produced signal. In the data sheet it mentions the Vbias to create an offset.

    However- is…

  • Timer Config ADUCM3029

    Hello. I have a simple code below that generate PWM with GP2 Timer2 Config and uses the GPIO33 pin of the ADUCM3029. Well, can you help me to configure the code that instead of usingTimer2 it will use the Timer1 (GPIO27 pin of the IC). I'm bit confused…

  • RE: ADUCM3029 pinmux document

    Hi Matt,

    If you are using the Cross Core IDE the pin muxing is located in the system.svc file at the bottom of your project assuming you already installed pin multiplexing add-in. By this add-in, you just simply select the peripherals to enable and this…

  • ADuCM3029 DAC DC Offset

    Hello,

    I am using the ADuCM3029. 

    While in both the low and high frequency loops, 

    When I produce a DAC sinusoid output signal, I measure through an oscilloscope to be a DC offset in the produced signal. In the data sheet it mentions the Vbias to create…

  • ADuCM3029 hello world example.

    Hi,

    I'm new to ADuCM3029. I'm running a "hello world" example from Keil IDE, but it doesn't seem to work. I have two issues:

    1. I'm expecting to see the print("hello world"), but didn't seem to execute the line. 
  • SPI Flow Control in ADuCM3029 not working

    Hello All,

    I´m developing a solution using 2 MCUs. The slave is wake up from SPI request and needs some time to deliver data to the master (Data just is transferred from slave to master). Because slave needs delay to start delivery data, I tried to apply…