• When build the target board with ADuCM3029/ADuCM3027

    Hello,

    Let me clear about development and flash writing for the target board with ADuCM3029/3027.

    1) For developing with the target board, which combination will work?

       A) CCES + ICE-1000/2000 : work (do you have any PCB design guide for this?)

       B) CCES…

  • RE: About the rewriting of firmware via UART(ADuCM3027)

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADUCM3027 Arduino Support - IDE

    Hello

    is there support by ADUCM3027 for Arduino IDE?

    Or Arduino compatible eval board?

    Thanks and Regards

    HU

  • RE: MMR Address Map for ADuCM3027/29

    Hi Macrip,

    This information will be added in the latest Hardware Reference Manual. There is still no release date for the document.

    Kind regards,

    Monica

  • Is there a tool to develop on Linux for the ADuCM3027/29 ?

    How can I develop with the ADuCM3027/29 on Linux?

    I used to use i.e. the GDB-Server for J-Link and can use most of the available tool-chains on Linux.

    I.e. Eclipse or Code::Blocks.

    I don't see the part supported with the GDB-Server for J-Link or Open…

  • RFPD-RC-4450-50

    The block diagram for the RFPD-RC-4450-50 shows the analog voltages from the power detector (Forward, Reverse, and VSWR) going to the ADUCM3027 but the schematic shows them going to the AD7293.  Which is correct?

  • Add user space CRC to hex file using CrossCore IDE

    I am working with the ADuCM3029 MCU and, for my application, I need to verify the user code integrity. I have been following this user guide (https://www.analog.com/media/en/technical-documentation/user-guides/ADuCM3027-ADuCM3029-User-Guide-UG-1091.pd…

  • User code CRC generation on CrossCore

    I am working with the ADuCM3029 MCU and, for my application, I need to verify the user code integrity. I have been following this user guide (https://www.analog.com/media/en/technical-documentation/user-guides/ADuCM3027-ADuCM3029-User-Guide-UG-1091.pd…

  • MMR Address Map

    The address of the different registers present on the ADuCM3029/ADuCM3027 devices are listed on the last chapter of the Hardware Reference Manual. The chapter is called “ADuCM302x Register List”.

  • Signatures and User Code CRC

    Hi, I'm working with ADUCM3029 and I read in "ADuCM302x Ultra Low Power ARM Cortex-M3 MCU with Integrated Power Management Hardware Reference Revision 1.0" and "ADuCM3027/ADuCM3029 User Guide" that there are two similar features: Signatures and…