• ADuc832 EEPROM

    We use the ADuC832 in a sensor that is in a remote location in northern Canada.  About once a week, a technician goes and powers up the sensor reads the sensor data.  In the ADuC EEPROM, we store some factory loaded calibration constants that never change…

  • ADuC832

    ADUc 832 and 842 microcontrollers. I there a way of locking the code so that other people cannot look or download the code?

  • Aduc832 crystal

    Hello:

    Aduc832 crystal  uses 32.768KHz watch crystal .The problem is, the frequency locking of aduc832 is inconsistent. When entering the download mode, the default BPS is 9600.  the serial port waveform from oscilloscope, each bit width is sometimes 82us…

  • ADUC832晶振

    你好:

    ADUC832晶振使用32.768kHZ钟表晶振,遇到问题ADUC832锁频不一致,当进入下载模式,默认比特率9600,832发送数据从串口波形上看,每位宽有时为82us、94us、110us。

    我使用晶振福电容为12.5pF,832内部集成18pF,所以我外部接电容经过几个容值电容的试验,都有如上问题。

    请帮我解决问题,谢谢

  • On ADuC832 DMA

    Hi Guys,

      Hope you are well.

      I have some problems on ADuC832 DMA. Would you like to help me?

      On DMA from the datasheet, there is some mentions as the following:

              "To enable DMA mode, Bit 6 in ADCCON2 (DMA) must be set. This allows the ADC results…

  • ADUC832 晶振问题

    你好:

    ADUC832晶振使用32.768kHZ钟表晶振,遇到问题ADUC832锁频不一致,当进入下载模式,默认比特率9600,832发送数据从串口波形上看,每位宽有时为82us、94us、110us。

    我使用晶振福电容为12.5pF,832内部集成18pF,所以我外部接电容经过几个容值电容的试验,都有如上问题。

    请帮我解决问题,谢谢

  • ADUC832- Flash data corrupted byte

    Hello

    Using the ADUC832BSZ62-5

    ESS Test were performed

    Procedure:

    System is ON.

    Cooling up to -54 deg and then switching OFF.

    Switch back to ON after some
    time.

     

    Problem:

    Program fails at startup during boot sequence : Check sum error/

    Preforming…

  • ADuc832/842 Hand held programmers

    Does anyone know of a hand held programmer for the ADuC 832/42 series of microcontrollers?

    We also use the Atmel ATMEGA128 series and are able to program this in the field using an Equinox-tech programmer.

    www.equinox-tech.com.

  • Read flash contents from ADuC832 device

    Hello,

    As the title suggest we need to get the flash contents from an ADuC device.

    According to these posts(same family chips):

    https://ez.analog.com/message/17287?q=read%20flash 

    https://ez.analog.com/message/24546?commentID=24546#comment-24546?q…

  • ADuC832 Debugging problems with Watchdog on.

    When I am debugging my ADuC832 code I get occasional completely wrong behaviour.  It seems to suddenly jump to code it should not go to at that time.  I have isolated the fact that this behaviour happens when I have the watchdog enabled.  What could cause…