FAQ
we want to use the USB-I2C_LIN-CONV-Z(MCV combi DONGLF) along with the I2CFTWSD.exe program to program Aduc7023. The driver of the "Aduc70xy USB-combi-Downloader" has been setup successfully.However, when running this program, it is unable to communicate…
Hi Sir,
About ADUCM7023 IC, Whether the ADUC7032 has ADC calibration in FT test ?
Thanks
Hello,
I am currently working on the ADUC7023 microcontroller and I am using the NI USB-8452 for programming.
I am wondering what could be the consequence of programming the flash memory without erasing all the flash memory before ? Could it be critical…
Hello,
I am using the dongle device (I2CWSD) and the NI USB-8452 device to program the ADUC7023 via I2C.
The following description is for the NI USB-8452.
I have checked the AN-806 Application Note which provide the different commands in order to erase…
programmer : jlink v9
programmer software:JLink_V645a
JTAG interface : TDI TDO TMS TCLK TESET
JTAG is used as a plain GPIO, and the address of 0x800014 is not 0xFFFFFFFF.
All caused by now can not erase the chip to download again,
is there any way…
I just got an ADuC7023 and a mIDSA-Link not long ago from ADI,but mIDSA-Link just can NOT connect ADuC7023 ,.
Jtag cable is good, ADuC7023 VDDIO is good, Reset ping is good, even i pressed Reset button and connected,it is still failed.
Somebody can help…
Is there source code available for a Software UART on the ADuC7023? Another thread from 9 years ago referred to an appended .c file but it does not appear to be available anymore.
在使用 ADUC7023 内部温度传感器测量温度时,读内部的温度ADC采样值,一直读会有个别ADC变动比较大的现象;请问是否有用ADUC7023内部温度传感器测温的参考代码实例?是否有下载链接?
Hi,
I am currently using the I2C of ADuC7023 as slave. As stated in page 60 of Rev G (link below), "Clock stretching can be enabled by other devices on the bus without causing any issues with the ADuC7023. However, the ADuC7023 cannot enable clock stretching…