• ADXRS649

    I was wondering if there was any source code or sample code that was available for the ADXRS649. We are using a chipKIT Max32 microprocessor and we are experiencing some difficulty trying to program that xy axis accelerometer when we thought this would…

  • About ADXRS649 gyros

    Hi,

         I am interested in using ADXRS649 gyros for an industrial application. Just wanted to know the following:

              1) Will the performance degrade if I use them to sense the angular rate in the horizontal "Y" axis, basically "pitch rate" rather than the…

  • ADXRS649 Calibration Options

    I need to calibrate an instrument that uses the ADXRS649 (+/- 20000 °/s) rate gyro.  This gyro will be used in a rate sensing application and will not be in a closed control loop so we need pretty good accuracy in the calibration scale factors (>= 1% of…

  • ADXRS649/UG-306 Cap size

    For the ADXRS649 eval board: UG-306, does anyone know the size of the capacitors on the eval board?  I was hoping to change C3 so that I can open up the bandwidth from the configured 10Hz to 1kHz.  Does anyone know how hard this solder job would be?

    T…

  • ADXRS649 Angular Velocity and Acceleration

    I am interested in using the ADXRS649 to measure angular velocity and acceleration.

    Based on the specifications, I believe that the sensor will be sufficient to measure angular velocity, but I was wondering if I could differentiate signal to get angular…

  • ADXRS649 Gyro and angular position

    Are there any app notes on how to integrate the rate signal of a ADXRS649 to obtain an angular position?

  • Minimum Supply Voltage for ADXRS646 and ADXRS649

    What is the minimum supply voltage for acceptable operation of the ADXRS646 and ADXRS649?

  • ADXRS649低温启动问题??

    做了个ADXRS649的测试板,做温度性能试验,从常温到-40度,一切正常,输出2.52V.新来实习的一工人,不知道操作,在低温-40度时给仪表断电了,再通电,输出2.6V左右,无陀螺功能,恢复常温过程中,恢复正常输出.

    做了多个测试板,只有一个有此现象,请问ADI专家,怎么会发生这种情况?

    再问一个,发现649全温标度因数的散布很大.买过两批,第一批,全温变化都在1%左右,第二批,在2%~3%.这种情况正常吗?,

  • ADXRS649陀螺仪引脚相关

    ADXRS649所有引脚都有相同的两个,电路板上该怎么配置呢?还有Vratio引脚可以接3.3V吗,麻烦了解的朋友解答下,谢谢!

  • Is there any example code for the ADXRS649?

    I am looking for some example code for the ADXRS649 or the EVAL-ADXRS649Z