We currently use the ADXRS610 in our products. Our manufacturer cannot get these and has suggested we use the ADXRS620. THe spec sheets are virtually identical except for the following statement, the ADXRS610 states, "A single external resistor can…
We currently use the ADXRS610 in our products. Our manufacturer cannot get these and has suggested we use the ADXRS620. THe spec sheets are virtually identical except for the following statement, the ADXRS610 states, "A single external resistor can…
According to the datasheet of ADXRS620, the output is proportional to Vratio, but the typical input range of Vration is not clearly given. I wonder whether it is possible to choose an ADC with its reference output - 4.096V as the input of Vratio. Moreover…
Hi
I use LTC1408 (ADC) to convert ADXL325 and ADXRS620 analog signals. LTC1408 ask to use a buffer amplifier before ADC to transform the analog signals, which have high source impedance.
ADXL325 has an output impedance of 32k for LP filter, so it is…
Hi,
I want to use the ADXRS620 with an ADC with an Full Scale output voltage of 2.5v.
As far as I can see, there are two ways I can do this.
adxrs620输出范围怎么调理到适合stm32f103的adc量程了?stm32f103是3.3v供电的。620输出我想加一级rc的滤波带宽控制在300hz内即可。
ADXRS652指标中,有一项Rate Noise Density是0.06°/s/√Hz,是否意味着ADXRS620的bandwith越大,噪声也就越大?譬如把BW设为2500,噪声就是0.06*√2500=2.5°/s?请问这样理解对吗?
另外,
如果我们采用16bit的AD,则理论的分辨率可以到0.0127°/s,如果因为上面BW过大导致噪声过大,那采用16bit的AD就没有意义了;
如果BW是80Hz,噪声也是0.05°/s左右,那这种情况下,16bit的AD足够,24bit的AD就很浪费…
ADXL78 |
ADXL001 |
ADXL278 |
ADIS16223 |
ADIS16240 |
ADIS16209 |
ADIS16203 |
ADIS16201 |
ADXL193 |
ADISEVAL |
ADXL1005 |
ADIS16000 |
ADIS16210 |
ADIS16227 |
ADIS16228 |
ADIS16229 |
ADIS16305 |
ADXL1001 |
ADXL1002 |
ADXL1004 |
ADXL103 |
ADXL151 |
A… |
Hello,everyone.I get a question about the ADXRS620's baudwidth.If we sample the ADXRS620's value every 1ms, how to set the baudwidth to get the best performance。
Thanks.