question1:数据手册中就只给了,RATEOUT随着顺时针旋转增加,没有给出具体的线性公式,我如何能从电压值换算位速率。
question2:为何要将C1 和C2短接到一起
希望大佬解答,提前谢了。
question1:数据手册中就只给了,RATEOUT随着顺时针旋转增加,没有给出具体的线性公式,我如何能从电压值换算位速率。
question2:为何要将C1 和C2短接到一起
希望大佬解答,提前谢了。
hello,i have a question about that why you connected E6 and E7 , G6 F7,.....,what's the function?
I was using ADXRS620 for my angular rate measurement.
Since ADXRS620 is NRND, is ADXRS642 compatible with my 620, ie, in the same PCB (layout) used for 620 can I get same functionality with 642 (compatible in mechanical, electrical pin-outs, electrical…
Hi:
I have some ADXRS620 ,and i make the PCB by myself ,also i solded the PCB with my Reflow soldering machine .But I fand that some of them do not work, the output always about 2.5V when i move zhe ADXRS620. I measure and fand that the voltage between…
技术人员您好:
我买了几个ADXRS620wba的传感器,使用回流焊焊自己做的PCB板上,发现有的能正常工作,有的不行,输出就2.5V,不会变化。
1. VDD,AVCC,Vratio使用的电源是单电源+5V供电,TS1,TS2,TEMP,NC引脚两两互联,没有外接。
2. 测试对比发现,正常工作的模块,D6,D7引脚上CP5-0.1uF电容两端的电压为16V以上,而不正常工作的模块CP5两端电压较小,有的2V多,有的8V,不确定,但远远低于手册上提到的电荷泵充电到的18—-20V。
…Hi, I just get another three question about the ADXRS620:
1. Based on the figure1 in the data sheet, may I conclude the drive axis utilize the trans-impedence circuit while the sense axis employ the charge amplifier circuit to sense the variation of…
技术人员:
您好!
我通过不同的渠道采购了两批次的ADXRS620芯片,但测试发现,两批次芯片的sensitive不相同,一种是6mv/deg,另一种是7mv/deg.
观察两个批次芯片正面的标记,发现主型号标示都是ADXRS620BA,,但其他三处标识有不同,包括中部的数字,左上角和右上角的字母和数字。
请问,ADXRS620芯片上的四处标识都是什么含义?怎么获知芯片的型号从而确定其sensitive?
通过查看手册,发现ADXRS622,ADXRS642的sensitive为7mv…