• How to calculate the measurement accuracy of ADXRS290 and ADXRS450?

    In datesheet,only Sensitivity of LSB/°/sec is given.(200 for 290 and 80 for 450)

    Can you give an example of calculating the measurement error by measuring a certain value, such as 10°/sec?

    Thanks a lot.

  • one external diode and one external inductor for three ADXRS450s

    I am going to use three ADXRS450s on my board. Can I connect VX pin of three ADXRS450s together, connect CP5 pin of three ADXRS450s together, and just use one external diode and one external 470uH inductor?

  • one external diode and one external inductor for three ADXRS450s

    I am going to use three ADXRS450s on my board. Can I connect VX pin of three ADXRS450s together, connect CP5 pin of three ADXRS450s together, and just use one external diode and one external 470uH inductor?

  • ADXRS450 蓝牙 应用 节能

    你好!

    我的工程是用ADXRS450 测量数据,通过蓝牙传输出来,在不测数据时蓝牙休眠,希望ADXRS450 也处于节能状态。

    有什么办法使ADXRS450 处于节能状态?

    有什么设置吗? 还是可以有什么电路可以关闭ADXRS450的供电?

    谢谢了!

    20200521

  • ADXRS450速率读取问题

    你好,我用STM32F103单片机读取ADXRS450的角度信息时遇到了一些问题。目前,我可以正确读出陀螺仪的PID和温度值,但在读取速率时静止状态陀螺仪返回值为0X4E08B460左右,参照SPI格式,得到返回的数据为0X45E3,除以80后转换为角速度为222.83°/s,数据明显存在问题。但当我转动陀螺仪时数据也会发生变化,所以应该是我数据处理上出现了错误,但是我未能找到错误,还请帮忙解答,谢谢!

    float GetGyroYaw(float IMU_T)
    {
      short res=…

  • RE: ADXRS450-temperature sensitivity

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADXRS450 Request error, PLL failure, Nonvolatile memory fault (NVM)

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADXRS450 Inductor Selection

    Q1 ) What is the range of inductor values suitable for 3.3v power supply? it recommends 540uH but what about using 680uH one?

    Q2) I am going to use a shielded inductor for my application but lowest cost one is 540uH with 30% tolerance (Automotive grade…

  • RE: ADXRS450 Digital Gyroscope : Needing help to generate 24V on CP5.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Help ADXRS450 5V and 3.3V power

    Hello

    For ADXRS450 gyro, is it possible to possible to provide 5V for boost regulator and 3.3V for others as shown in image? The intention is to reduce the noise on power supply plane due to switching regulator.

    Since output of 5V and 3.3V sources are…