FAQ
There are two options for evaluating the ADXRS290. One is a simple breakout board (EVAL-ADXRS290Z) and the other is a GUI based real-time evaluation system (EVAL-ADXRS290Z-M/M2).
The EVAL-ADXRS290Z allows for quick evaluation of the ADXRS290 dual-axis…
The EVAL-ADXRS290Z-M/M2 is an easy-to-use evaluation tool targeting bench or desktop characterization of the ADXRS290 gyro. The system contains the inertial sensor evaluation main board (ISEB) and the EVAL-ADXRS290Z-S or S2 satellite board. In addition…
Hi JCSO,
the bias does change with temperature, figures 5 and 8 of the datasheet show the sensor output vs temperature for multiple parts.
Pablo.
In datesheet,only Sensitivity of LSB/°/sec is given.(200 for 290 and 80 for 450)
Can you give an example of calculating the measurement error by measuring a certain value, such as 10°/sec?
Thanks a lot.
Hey there,
the selection table (https://www.analog.com/en/parametricsearch/11176#/sort=5100,asc) for gyro sensors states that the ADXRS290 has an angular random walk of typically 0.17 °/√hr, but I don't find any information regarding the random walk inside…
对于ADXRS290 如果想要在一次传输中想要读取到XD0 XD1 YD0 YD1,只需要发一次寄存器地址之后保持CS信号拉低一直给8*4=32个sclk信号就可以吗,还是要像ADXL345 一样把A6置成1再进行连续传输
What is the output voltage of the filter circuit on page 12 of the ADXRS290 datasheet when the sensor is at rest? The datasheet only gives the sensitivity (5 mV/(deg/s) but not this at-rest level. Might be useful to add it to a future revision of the…
ADXRS290使用一段时间后陀螺寄存器数据不对,静止在桌面时,陀螺数据随机跳动,而且很大,从0到200多度每秒都有。
这种情况大概和什么有关,比如震动?高温?泡水?
Datasheet says sync pin is kept high until the data is read but it doesn't say clearly that it stops updating data registors. In other words what happens when the gyro gives an interrupt but we wait before reading the data