• ADXL78 temperature coefficient

    Our customer used ADXL150, ADXL105, ADXL190, ADXL250 and ADXL278 before, and
    she found the relation between the output and temperature is monotonic. That
    is: if the temperature increase, the output will increase too. Now she used
    ADXL78, and she…

  • ADXL78, ADXL278 Output Impedance

    Could you please let me know the Output Impedance of the ADXL278?

     

    The XL78/278 output impedance is pretty low – a few hundred ohms. Certainly
    less than 1k.

  • ADXL78有评估板吗

    ADXL78有评估板吗,官方没有价格是去代理那里询价吗

  • RE: ADXL78 output - RC

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Tag List: MEMS Inertial Sensors Tags

    The following is a list of parts this group talks about. Update as necessary.

    ad22282-a-r2, ad22290, adia16201, adis16003, adis16006, adis16203, adis16204, adis16209, adis16210, adis16223, adis16227, adis16228, adis16229, adis16240, adis16255, adis16265…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • RE: 有奖“示爱”行动——谈谈那些让你爱爱爱爱不完的电路

    ADXL50:MEMS加速度计的鼻祖,一款单片集成的MEMS芯片,采用差动电容作为敏感结构,采用静电力反馈闭环控制平衡电路,输出与对应加速度成正比的电压信号。

    现在已经停产,可用ADXL78代替,不过这也改变不了它的地位!!

  • RE: Need further clarification on the frequency response of the ADXL356.

    I was expected to be able to model the frequency response of the device to +/- 20% at 1.5 kHz including all variation due to the output filter and the structure. This does not include scale factor variations. The variations due to the structure at 1.5kHz…

  • AD22302 fourth generation i-MEMs : sensor axes orthogonal ?

    What is the difference between MEMs and i-MEMs ? In the datasheet of the AD22300 serie Automotive i-MEMs, it describes those accelerometers as derivative products of the fourth generation ADXL78 family surface micromachined i-MEMS accelerometers. How…