Hi,
.
How to determine the g value from adxl377 based on action/ shcok. or how to verify the g value received from accelerometer--adxl377.
Could you please tell me what the typical damping factor is for the ADXL377 accelerometer?
I seen a similar post to mine was answered but for the ADXL325 and ADXL326 accelerometers, in that answer it was said them accelerometers have an under-damped response…
Hi all,
A potentially silly question regarding the output of the ADXL377:
If the output for each axis is given as a voltage representing the current g's experienced by the device, how is a negative g' rating represented?
Is it given as a negative…
Does anyone have any tips on how to go about soldering leads to a micro ADXL-377. We are making an ear accelerometer and need to be able to solder several wires to this very tiny device.
any feedback appreciated.
Thanks,
Tony
I have an application where I plan to use the ADXL377 where the initial shock is 1000g for about 10 msec. I'm assuming that it will survive this shock, so what I need to know how fast the ADXL377 will recover from this overload.
Thanks....Steve
I'm working on a project that measures high impact. It seems that the ADXL377 is perfect for my application. I would like to sample all three axis' at full resolution and as high a sample rate as I can get. The actual measured impact will take less…
Hi, I'm using the ADXL377 on the evaluation board, and I was wondering what the output impedance of the x,y, nd z channels are on the board?
Thanks!
Hello,
in the case of an acceleration on Z axis of 180g (centrifuge acceleration), is ADXL377 able to measure correctly on X and Y axis?
I'd like to use it to measure vibrations.
Thanks
I would like to use an accelerometer ADXL377 with a power supply of 3.3V. I don't find its sensitivity for this value of power supply... How can I compute it? In the datasheet of the ADXL326, it is specified but it isn't in the datasheet of the…