• RE: adxl354, adxl354-eval outputs, relation to V_IP8ANA

    Thank you for posting your question in this forum.  Unfortunately, we have recently discovered some gaps in our support strategy, which are going to take us some time to fully address.  While we figure out who will cover this product, in this forum, I will…

  • RE: ADXL354 reading

    I use adxl354 on the new board.

    All signals are given as you wrote. But the outputs Xout, Yout, Zout are fed to the inputs of operational amplifiers and are equal to 0.

    What can be connected wrong?

  • RE: ADXL354 Connections

    Thank you for posting your questions in this forum. 

    From what I understand, we characterized these devices using an approach that is based off of #1, on your list.  Having said that, it is difficult to offer preference for one approach, or the other, without…

  • ADXL354 reliability

    Hi All,

    We use ADXL354 to replace ADXL203 recently. Our product is detecting vibration, shock can up to 500g. We can care about the vibration start or not. So high shock range is not suitable for us. 

    We found ADXL354 sensitivity drop down for some time…

  • ADXL354 Temperature Conversion

    Hi to all,

    I'm working on an ADXL354 analog accelerometer with internal temperature sensor; the accelerometer values are ok but I can not correctly convert temperature voltage output in Celsius degrees.

    What I make is:

    Temperature [°C] = 25  +  (…

  • ADXL354 output

    Hi, 

    I'm using the EVAL-ADXL354 board in a new project. I connected it to a ADS1256 to read values. I'm new to this types of devices but reading the docs I understood that when the sensor is motionless (in conditions of 0g) I should read in output a value…

  • ADXL354 Noise Density

    Hi,

    Looking into ADXL354 datasheet, I found 20 ug/sqrt(Hz) noise density value. Is this value the same for each measurement range? (±2g , ±4g ,±8g ) . If not the same, please can you explain the values for each range?


    Also Which frequency range is this…

  • ADXL354 System Noise

    Hello,

    I am currently working on a project that has this requirement: Accelerometer RMS Noise: System noise shall be less than 40 µg measured over 0-30 Hz

    I am now looking at the ADXL354 datasheet. I found out that the Noise Density at +- 2g range…

  • ADXL354 signal

    I have recorded  these 2 signals coming from a shot. Acquisition parameters are the same; the board containing ADXL354 is fixed firmly to an externa box, in strong contact to  ground.

    The differance between signals is great, i think my procedure has something…

  • ADXL356 ADXL354 Frequency Response

    Hi

    I have a question about the ADXL 356, ADXL 354 data sheet.
    Does the graph on Frequency Response reflect the internal filter, or is it the bare characteristic of the MEMS sensor?
    I guess this is a naked character.

    Data Sheet ADXL356/ADXL357 (Rev. 0…