• RE: How to solve problems communicating with an ADXL345, ADXL346 or ADXL350 via I2C.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: How can you distinguish between the ADXL345 and ADXL350 via the SPI / I2C Bus?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Can the ADXL345 driver be used with an ADXL350?

    Hi,

    I want to use the ADXL345 "generic" driver with an ADXL350 in SPI mode. I'm hoping there's enough similarities to use the generic files:

    ADXL345.c

    ADXL345.h

    Communication.c

    Communication.h

    Besides the obvious changes, i.e.…

  • 请教ADXL350的偏置问题

    刚刚开始学习的菜鸟新手提问,希望得到ADI工程师和前辈的回答。

    入手一块ADXL350的开发板,使用STM32F4,SPI四线通信。  现在通信没有问题,但是收到的数据有一些问题,如下图:

    其中[0]、[1]、[2]分别为X、Y、Z轴的数据。

    这是模块平放(+Z)时的数据:

    模块反放(-Z)时的数据:

    +X方向放置的数据:

    -X方向放置时的数据:

    +Y方向放置时的数据:

    -Y方向放置时的数据:

    从数据中可以看出,数据变化的方向是正确的,XY轴的数据相对较为准确…

  • ADXL350

    Hi,

    I'm using a ADXL350 in my design to detect the motion of my hardware. I have some trouble to understand how to set up the OFFSET for the three axis. I understood I should read the output for X Y and Z (command 0x32 and followings) first and then…

  • RE: ADXL350 evaluation board documentation

    I am sorry that this post was missed.  Unfortunately, our support model for these products had substantial weaknesses, when we first launched this forum.  We are addressing those weaknesses now and will respond to any future requests, much quicker in the…

  • ADXL350最简初始化问题

    我用的ADXL350的程序如下:

    void main(void)

    {  

        WriteToADXL350ViaSpi(0X31, 1, 0X2b);  // DATA FORMAT  +-8G 右对齐 中断低电平有效       0010 1011

        WriteToADXL350ViaSpi(0X2D, 1, 0X08);  // POWER on standby

        WriteToADXL350ViaSpi(0X2E, 1, 0X80);  //  中断

        WriteToADXL350ViaSpi(0X2f…

  • ADXL350 所能测量外界振动的频率是多少?

    ADI工程师:


            ADXL350 内存刷新的速率是3200Hz,那我测量100Hz的信号的话,每个周期的传感器采样点数就是32个,我可以这样算么?

                                           

  • ADXL350通讯速率问题

    数据手册上写的:输出数据速率3200,带宽1600。

    请问:


    这个速度是提供给主机通讯的最高速率么?还是350内部的采样速率?

    如果是主机通讯速率,我现在示波器上看见的单片机通信的速率是1785Hz,是不是通信的太快了?


  • 寻找ADXL350的Linux驱动

    rt

    我们新的产品上正在使用adxl350的三轴加速度计,使用的Linux内核版本是3.2.0

    在内核中没有发现adxl350芯片的驱动,在adi官网上也没有发现。

    想请问如果这个芯片有官方的驱动,能否附件共享一下?

    主推的芯片不会没有驱动吧。

    谢谢。