• ADXL350 - Non-operation at high temperature

    < It's related to non-operation at high temperature >

    When the surface temperature of the ADXL350 is 40°C or higher, the register is not read/write when the power is turned on/off.
    In this state, it is maintained even when the JTAG debug is…

  • ADXL350 Abnormal behavior

    Hello, I'm Dohwan Kim. I'm a Korean.
    Please understand that I am not good at English.

    Our company used the ADXL350 to make a Roll Data measuring device. 200 units a year were produced for 3 years, and there are plans to continue production for…

  • ADXL350 static acceleration

    Hi

    I am using ADXL350 to detect the angle of rotation for certaim range. Eg. 0 to 60deg, but sometime data is over-range. may be because the data include dynamic acceleration (due to vibration). Is it possible to measure only static acceleration?

  • ADXL350: Where can I find the user guide for ADXL350 Evaluation System?

    Where can I find the user guide for ADXL350 Evaluation System? It is not on
    ADXL350 page on www.analog.com

     

    Please see attached Rev 0 of the EVAL-ADXL350Z-M User Guide. This user guide
    will be posted to our website shortly. (Please…
  • ADXL350 ADC condition

    Hi

    ・About ADXL350, are there digital filter AC characteristics data ?

    ・How Hz is internal clock dipersion and ADC sampling rate?

        Because simultaneous data is required.  

    Best regards

    Thank you very much

       

  • ADXL350 for Digital Angle Meter?

    I'm sure everyone has seen those small digital angle meters with reported accuracy typically 0.1 or 0.2 degrees. I'm looking to design something that can have an accuracy of 0.05 degrees and I think perhaps the ADXL350 might be a good candidate.…

  • RE: Layout information of ADXL350

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADXL350 SPI 4-wire communication problems

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • The ADXL350 uses SPI readings occasionally with errors

    The ADXL350 recently encountered reading problems. The controller uses the timer to read
    1024 data regularly in 1 second, but sends the data to the host computer and finds that
    the data has the jump error. As shown below: Yellow: Z axis, purple: Y axis…
  • RE: How to solve problems communicating with an ADXL345, ADXL346 or ADXL350 via I2C.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,