• Absolute Maximum Voltage of ADXL326

    Hi,

    Let me know about Xout and Yout absolute maximum ratings.
    Absolute maximum ratings is written that all other pins is (COM − 0.3 V) to (VS + 0.3 V) .
    However, Figure22 seem to exceed the absolute maximum ratings. I also confirmed this phenomenon…

  • ADXL326 frequency response drop seriously

    Hi ADI guys,

      We test ADXL326 recently as our new project application for low-frequency vibration ,and find there is some  frequency response problem,

      We test X axis ,when the frequency  exceed 500HZ, the acceleration magnitude drop seriously, as below…

  • ADXL326 Power usage & weight

    I would like to know what are the power usage (in Wh) & weight of the ADXL326 accelerometer.

    Many Thanks

  • ADXL326传感器频率响应不线性的问题

    用ADXL326做传感器,主要用到Z轴,带宽限制已经弄到1kHz以上了,采样率8k,在0-200Hz的时候,精度很好,到了200Hz以上,加速度值就偏小得多。不知道什么原因?板子是直接固定在金属件上的。

  • ADXL325 and ADXL326 acceleration difference

    Hi,

    I am using ADXL326 EVK in my designs to measure the acceleration of an Actuator. For the verification, I tried to use the other accelerometer ADXL325 to get G peak values. Strangly observed totally different results.

    As per the datasheets ADXL326…

  • ADXL326 accelerometer footprint

    Hi There,

    I'm trying to use the ADXL326, but in the footprint below:

    On the right side there is the size of the internal pad (mentioned in the datasheet to mechanically strength the device to the board). But the possible size stretch from 1.08…

  • ADXL325 and ADXL326 different accelerations for same setup and same input signal

    Hi,

    I am using ADXL326 EVK in my designs to measure the acceleration of an Actuator. For the verification, I tried to use the other accelerometer ADXL325 to get G peak values. Strangly observed totally different results.

    As per the datasheets ADXL326…

  • EVAL-ADXL326

    How can I control X,Y, and Z frequency spans. Accelerometer is only measuring till 50Hz only.

    I believe I have to do something to the capacitors C1, C2, C3, and C4.

  • RE: adxl326 calibration curves and sensitivity

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,