• ADXL322: Offset specification

    For an automotive application I need to have just a confirmation.
    The "0 g Voltage at Xout,Yout" in the "Zero g BIAS LEVEL" specifications on the
    ADXL322 data sheet, have a value from 1.3V to 1,7V.

    This value is also the maximum…

  • Should I connect the ADXL322's EPAD to Gnd or leave it floating?

    Should I connect the ADXL322's EPAD to Gnd or leave it floating? This
    information is missing in your datasheet.

     

    It’s not necessary to connect the external pad (EPAD) to ground.  It is purely
    for mechanical rigidity and can be left unconnnected…

  • ADXL213: Magnetic field area

    Can the Accelerometer ADXL213 work in a magnetic field area?

     

    The sensor in the accelerometer is a polysilicon surface-micromachined
    structure built on top of a silicon wafer. The operation of the accelerometer
    is unaffected by magnetic fields…

  • Tag List: MEMS Inertial Sensors Tags

    The following is a list of parts this group talks about. Update as necessary.

    ad22282-a-r2, ad22290, adia16201, adis16003, adis16006, adis16203, adis16204, adis16209, adis16210, adis16223, adis16227, adis16228, adis16229, adis16240, adis16255, adis16265…

  • RE: 这些网红healthcare产品背后的“ADI Inside”知多少

    UTAS案例采用器件:

    Blackfin对称多处理器ADSP-BF561——https://www.analog.com/cn/products/adsp-bf561.html

    Zoll Medical案例采用器件:

    iMEMS®加速度计ADXL322——https://www.analog.com/cn/products/adxl322.html

    OrthoAlign案例采用器件:

    iSensor® MEMS 惯性测量单元 (IMU) 传感器…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • how do we measure non-linearity of G-Sensor

    Take ADXL322 as example, the non-linearity spec is +/-0.2% of FS, how we run the measurement? is there a simple setup for the spec?

  • EVAL-ADF70XXMBZ2

    hi,

    May I ask for a copy of the source code of chip programming software which

    display the data received by the EVAL-ADF70XXMBZ2 connected to a host PC transmitted by another EVAL-ADF70XXMBZ2 via RF

    which Analog Devices created?

    Both EVAL-ADF70XXMBZ2…

  • adf7021-N

    hi everyone;

    my name is harsha ;i wanted to program adf7021-N eval board with msp430F5438A experimental board . the interface part is the problem the header jacks are not identical so can anyone suggest me how to connect them reliable what the way and…