FAQ
In the early stage, I used the ADXL213 sensor to build a circuit to realize the Angle of inclination. Since the installation is not from the center of the circle, the Angle of inclination fluctuates within the range of 0° to 20° in the process of non-uniform…
Hi, I have been using the ADXL213 in a low volume, specialist hobby application that has been working well across the world exposed to the elements and wanted to build a new batch of 5 units but was shocked at the ~$35 price.
I need help finding a more…
We are using the ADXL213AE from many years with very high results . Our main applications are : Platform leveling , cranes , aerial work platforms and many mobile applications . The inclinomeers that we realize are very performant . For new applications…