• ADXL213: Magnetic field area

    Can the Accelerometer ADXL213 work in a magnetic field area?

     

    The sensor in the accelerometer is a polysilicon surface-micromachined
    structure built on top of a silicon wafer. The operation of the accelerometer
    is unaffected by magnetic fields…

  • ADXL213 Dynamic Anglog measuring method

    In the early stage, I used the ADXL213 sensor to build a circuit to realize the Angle of inclination. Since the installation is not from the center of the circle, the Angle of inclination fluctuates within the range of 0° to 20° in the process of non-uniform…

  • ADXL202, ADXL203, ADXL213 - all dual axis accelerometers: Is it allowed to operate the 2-axis sensor (+/-2g) in a x-y plain, where in z-direction a high static

    Is it allowed to operate the 2-axis sensor (+/-2g) in a x-y plain, where in
    z-direction a high static
    acceleration (100g) is present?

     

    No damage will be caused to the accelerometer

    The datasheet (Absolute maximum ratings) says +-500g - with…

  • RE: ADXL213

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: caibration of ADXL213

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADXL213 Self-Test Response

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADXL213 possible noise sources?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Need help finding replacement for ADXL213

    Hi, I have been using the ADXL213 in a low volume, specialist hobby application that has been working well across the world exposed to the elements and wanted to build a new batch of 5 units but was shocked at the ~$35 price.

    I need help finding a more…

  • ADXL213 REPLACEMENT

    We are using the ADXL213AE from many years with very high results . Our main applications are : Platform leveling , cranes , aerial work platforms and many mobile applications . The inclinomeers that we realize are very performant . For new applications…