• ADXL206: Vibration Rectification Error

    I am interested in finding out more about the ADXL206's performance in high vibration environments. Specifically, is there a specification for the Vibration Rectification Error (VRE)?

    Thanks!

  • RE: ADXL206 Axes

    We are sorry that this was missed.  The current ADXL206 datasheet shows this in Figure 3 on page 5.

    http://www.analog.com/media/en/technical-documentation/data-sheets/ADXL206.PDF#page=05

  • RE: ADXL206 output question

    It looks like this question was missed, and the organization around this forum has undergone several changes ever since. Sorry about that.

    If you are still unsure, When the arrow is oriented downwards (in line with earth's gravity), the X axis output…

  • RE: operating voltage range for ADXL206

    By the way, if you must use the ADXL206 outside of its specified conditions, I would recommend validating this in your testing. Good luck!

  • Tag List: MEMS Inertial Sensors Tags

    The following is a list of parts this group talks about. Update as necessary.

    ad22282-a-r2, ad22290, adia16201, adis16003, adis16006, adis16203, adis16204, adis16209, adis16210, adis16223, adis16227, adis16228, adis16229, adis16240, adis16255, adis16265…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • RE: 盘点那些突破高温桎梏的器件们~

    高温器件一览

    AD5600 高温、16 位、非缓冲式电压输出 DAC、SPI 接口
    AD7981 耐高温、16位、600 kSPS PulSAR® ADC
    AD8229 1NV/√HZ低噪声、210°C仪表放大器
    AD8634 高温、低噪声、轨到轨输出双通道运算放大器
    ADG5298 高温(高达210°C)、高电压、防闩锁型、8通道多路复用器
    ADG798 高温(高达210°C)、低电压8通道多路复用器
    ADR225 高温…
  • RE: 高温器件怎么测试?ADI工程师告诉你直接放进烤箱里!

    高温iMEMS 加速度计ADXL206

    这是一款精密、低功耗、完整的双轴iMEMS®加速度计,提供13 mm × 8 mm × 2 mm、8引脚侧面钎焊陶瓷双列直插式封装(SBDIP),适用于高温环境例如井下钻探。这款加速度计将传感器和经信号调理的电压输出集成在一个单片IC上。满量程加速度测量范围为±5 g,既可以测量动态加速度(例如振动),也可以测量静态加速度(例如重力)。典型本底噪声为110 μg/√Hz,因而在倾斜检测应用中,可以利用窄带宽(<60 Hz)解析1 mg(0.06°倾斜…

  • RE: ADXL 206 higher G rating?

    I probably should have described this a little differently.  The core used in the ADXL206 is capable of this, but the ADXL206 is not.  It would require a new product.  I am going to start a private discussion with you to discuss this in more detail.

  • RE: Is there an Eval board for ADXL206HDZ

    This forum is not for sales support. Please check through your ADI customer service channels for help in meeting your customer's needs.  I am not aware of any evaluation tools for the ADXL206.  Sorry about that.