FAQ
Regarding the ADXL206 zero G shifting, I conducted a test on a board with three ADXL206 on it one for each axis.
I set it up in an oven an conducted a temperature test wit a 1°C/minute ramp-up/down. I ran the test two times and processed the data output…
I'm using an ADXL206 in a board to detect the orientation of it, it should operate up to 150°C.
I laid out two prototype boards and started a test up to 135°C, they worked fine for a couple of hours and then I noticed that on one board the X axis…
I'm designing an electronic board for a downhole drilling application, i'm intending to use your ADXL206 Accelerometer.
What i can't find on the datasheet is any information on the centerline - ie i would like to position the sensor as close…
Again, sorry for the gaped coverage on this product. Your interpretation is correct, with one exception: we would anticipate a degradation model that is closer to a square root of time approximation. Hope that helps.
Hi,
I use ADC to read ADXL206 XOUT YOUT voltage with Cx Cy set as 1uF. On page 10 of the datasheet, there is a formula f(-3dB)=1/(2pi*32K*C), I calculate f(-3dB)=5Hz when C is 1uF . In the firmware I set ADC sampling rate as 10Ksps(sample per second…
Hi, I am using 2 ADXL206 chips to get 3 axis G readings, then convert to inclination angles using arc tangent formula. How do I perform the inclination calibration routine to match the calculated angle with the true angle? Is there any coefficients involved…
我想请教一下ADXL206的温度迟滞问题;
在加温试验中发现:当传感器位置一定时,假设温度从T0升温到T1时,在T1时刻的输出为Y1,温度从T2降温到T1时,T1时刻的输出Y2(0<T0<T1<T2<175),Y1和Y2不相等,其差值最大可达到满量程的1%(10mg),请问这个是ADXL206该有的现象吗?是不是加温曲线和降温曲线本身就存在一个滞环?