• adxl103 and adxl203 saturation recovery time

    For the adxl103 and adxl203, is there a graph of the output's recovery time once it has been saturated/shocked with varying degrees of magnitude up to the absolute maximum shock? Is there an internal reset that recognizes over/out-of-range activity and…

  • 单轴加速度传感器选型

    项目需要一款单轴加速度传感器,模拟量输出,量程5g以内,分辨率0.1mg. 目前仅找到一款ADXL103,但是好像分辨率有点低,麻烦问下有没有更合适。感谢。

  • Tilt sensing MEMs performance requriement

    if we have the lower noise parts on the roadmap to compete, their noise density
    is 50ug/Hz, while our best part ADXL103/203 is 110ug/Hz. (compete with
    LIS244ALH)

     

    comment on noise if Tilt measurement is the concern. 
    In principle customer has…

  • Tag List: MEMS Inertial Sensors Tags

    The following is a list of parts this group talks about. Update as necessary.

    ad22282-a-r2, ad22290, adia16201, adis16003, adis16006, adis16203, adis16204, adis16209, adis16210, adis16223, adis16227, adis16228, adis16229, adis16240, adis16255, adis16265…

  • 关于adxl03灵敏度的问题

    ADXL103的灵敏度问题,我看到以前提的问题:

    Q1:“The ADXL103/ADXL203 output is ratiometric, so the output sensitivity (or scale factor) varies proportionally to the supply voltage. At VS = 3 V, the output sensitivity is typically 560 mV/g. Sensitivity at XOUT, YOUT VS …

  • General PDN policy?

    I can 't seem to find a general statement from ADI concerning the PDN process, I believe I've heard that there's a 2-year window that is started by the PDN process, but is there a generic policy statement on this that I can share with a customer who's…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • RE: ADXL321 replacement

    Hi Mark,

    Wow. Appreciate the fast response.

    This is a new design, but it's a follow on of an existing design that used the ADXL203 and ADXL103 combination. The 2.5k BW and 110ug/sqrtHz parameters are what set this product apart from the rest.

  • What does "Not recommended for new designs" mean?

    To whom it may concern:

    Jewell Instruments has design in the ADXL103 into two major platform products which are being introduced this year.  When I was researching on your website today I was very much alarmed to see in the product's web page under Product…

  • How to compare noise levels between digital and analog accels?

    Analog accelerometers e.g. ADXL103, have noise levels quoted as micro-g-per-root-hertz. For that one it's around 100 micro-g/rtHz. This is a spectral quantity (i.e. it is the noise in a certain bandwidth).

    Digital accelerometers e.g. ADXL345 have…