I am sorry that your request did not received a response. Our support strategy for these forum had some gaps in coverage, which I was unaware of. We have addressed this issue and will be ready to respond much quicker in the future. The ADIS16362 uses…
ADXL 103 CE 加速度传感器能否测竖直方向的振动?该款传感器标着测试方向是水平面内的X或Y轴,我发现竖直放置使用时,零g偏移电平在3.5V,这样能可以正常使用吗?影响测量精度吗?是否有z方向的单轴加速度传感器?
I was wondering if anyone knows if one can leave an output pin completely open if you don't need the output signal. I understand that there will be a lot of clock noise on it. The data sheet almost threatens the worlds end if you don't put at 1nF or larger…
Hello,
I guess this question is directed towards someone at Analog Devices since it has to do with the long-term availability of the ADXL103/ADXL203 series of analog one- and two-axis accelerometers.
I noticed that the ADXL103 and ADXL203 are labeled…
“The ADXL103/ADXL203 output is ratiometric, so the output sensitivity (or scale factor) varies proportionally to the supply voltage. At VS = 3 V, the output sensitivity is typically 560 mV/g. Sensitivity at XOUT, YOUT VS = 5 V is 1000mv ” ,说明书上这两处,似乎有误…
Hi,
ADXL103/ADXL203 contains 0 g Offset vs. Temperature parameter. Did you specified 0 g Offset Long Term Drift (0 g Offset vs. Time)? If yes, where I can find the data?
Regards,
Ivan
输入电压为3.0V-3.6V,用的电源稳压芯片是MCP1253-33X50I/MS ,将电压稳定到5V后,ADXL103CE输出电压为2.3几到2.4几。
请问这是怎么回事?