• ADXL103: ADXL203

    Is the ADXL103CE Rohs compliant?
     
    The material declaration says 2.1milligramm PB

     

    The package is ROHS compliant until the year 2015.

    It is a process related exemption. The package contains a cap.

    To solder this cap at high temperatured Pb is…

  • ADXL103/203 Accelerometer sensitivity

    How does the sensitivity of the ADXL103 accelerometer changes with
    power supply voltage? What is the sensitivity if I supply 3.3V?

     

    Sensitivity is essentially ratiometric to VS. This means the output offset
    voltage and sensitivity will scale linearly…

  • ADXL103: Noise in accelerometer

    We are currently using some of your accelerometers to measure subsea pipe
    motions for offshore applications (extremely small motion amplitude ~ 0.01 m
    and reasonably low frequency 0.03 Hz). I have a few questions regarding your
    accelerometer's…

  • ADXL103/ADXL203 Sensitivity over frequency

    Can you guarantee that sensor output sensitivity is exactly the same when using
    at different frequencies?
    Can you provide sensitivity vs frequency characteristics for ADXL103 or ADXL203
    accelerometer sensor please?

     

    Unfortunately, I cannot confirm…

  • ADXL103: Root cause of temperature drift component

    What is the root cause of the "Temperature drift component (X-axis)". What is
    the definition specified as "typ" compared to "max". Is "typ" equal to 1 std
    dev? What I am requesting is more or less what is…

  • ADXL103 / ADXL203 accelerometer with AD7887 ADC for vibration sensing

    I want to measure vibration with an ADXL103/ADXL203 accelerometer and sample the analog output voltage with an AD7887 ADC at a rate of around 2.5kHz. The samples are then used to calculate an RMS value (based on 5000 samples). The bandwidth of the accelerometer…

  • is an ADXL103 effected by a magnetic field?

    Want to use an ADXL103 and use a magnet to attach it. Will the field have any effect on the response?

  • Will it be possible to integrate ADXL103/203 in to a wearable with smartwatch

    I am interested to design a wearable  smartwatch with ADXL103. This will be a great Aid for disabled/Aged patients to detect a fall 

    Happy to connect/collaborate with any one. A potential Covid19 Solution also can be thought of.

  • RE: Question about ADXl103

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,