Hi ADI guys,
We use ADXL1005 for Machine bearing monitoring ,the noise density is 75ug/hz, We set the BW 10KHz, so the RMS noise is about 7.5mg,
We actually test the noise after MCU (read inner ADC raw data) is about 0.4mg,so whether the noise is well…
Thank you for your attention.
Our customer used to work with the ADXL150.Customers are now interested in the ADXL100X series.From the ADXL150 precedent, customers believe they need to know what happens when acceleration exceeds the operating range.
Best…
I will want to make EVAL-ADXL1005.
Could you give me a Gerber data of EVAL-ADXL1005
https://www.analog.com/jp/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-ADXL1005.html
I used ADXL1005 to monitor the vibration of Motors. How would I select the correct ADC IC to sample the analog output ADXL1005?
Please recommend the ADC Sensitiity ,Resolution,Sample Rate 。
And if I need FFT to analysis the freqency domain performance…
I was wondering if I could use ADXL1005 at a variable magnetic field (increase from 0 to 1 T in 1 s, then stable magnetic field for 1 s, then fast transient 0.1 T in 1 ms)?
Would you recommend any shielding for the accelerometer and/or cabling?
Thank…
Do these two evaluation boards include the sensors ADXL1004 and ADXL1005?
And which type of sensor is included in the evaluation board (ADXL1004BCPZ, ADXL1004BCPZ-RL, ADXL1004BCPZ-RL7)?