• About ADXL1003

    Hi there,

    I'm currently working on a research project of condition monitoring of engine. So for that I need to measure vibration signals of engine, for which I required minimum 8-10khz accelerometer sensor. I have found one of them i.e ADXL1003. I want…

  • ADXL1003 OR pin

    Hello, I have two questions on ADXL1003.

    Please give me advice.

    https://www.analog.com/media/en/technical-documentation/data-sheets/ADXL1003.pdf

    #1,  when you not use OR pin,  what should it be treated? I think it it output pin, so it should be treated…

  • EVAL-ADXL1003 BOM

    Board EVAL-ADXL1003 features output filter components R1, R2, C1 & C2.

    On the schematic they are "TBD", but there are parts fitted. Where can we find the values used?

  • ADXL1001,ADXL1003,ADXL1005,Overload response

    Do you have the following data about ADXL1001, ADXL1003, ADXL1005?
    1. Offset voltage stability when the device is exposed to increasing acceleration.
    2. Peak clipping level when the device is exposed to excessive acceleration.

    plesase.

    Best regards

  • ADXL1003相关问题

    我在ADXL1003后面接上一个ADC转换成数字量传给MCU,然后平放时读出来的加速度并非0g而是1.几g,(已关闭自检)我又试了它在x轴上的加速度,正反方向还算正常,两个方向相差有2g,我想问下平放时有1.几个正常吗?是设备的零漂吗?不正常的话大概是因为什么呢?谢谢!

  • RE: ADXL1001 Linear plot of sensitivity with voltage

    Hello  !

    No worries at all. My respect goes to you, as well! 

    Fortunately, FormerMember was available to confirm the Excel table that we created, for this purpose. I hope that this helps. 

    With respect to the power supply question, I noticed something…

  • RE: Can anyone suggest similar features MEMS sensor for the attached conventional accelerometer datasheet?

    Hi ,

    Can you elaborate on the exact specs that are important to your application? What exactly are you trying to measure?

    Analog Deviecs offer CN0532, a conversion board that allows MEMS sensors to be used with existing IEPE infrastructure …

  • RE: ADXL1003Z self-test

    Hi Darshen, 

    To build on Mark's answer here. The self test routine is described on page 10 of the datasheet: https://www.analog.com/media/en/technical-documentation/data-sheets/ADXL1003.pdf. It describes that you provide 5V at the VDD pin and 0V at…