• ADXL1001加速度计没有输出

    近期在使用ADXL1001加速度计时出现问题,具体表现为供电电压为5V时加速度计没有输出电压,所以我们无法判断是加速度计本身有问题,还是我们电路设计有问题,电路原理图如图所示,电源为15V,经RT9058转换为5V为加速度计供电。

    现有3种猜测:

    1、由于我们是手工焊的ADXL1001,怀疑芯片没有焊好

    2、RT9058输出电压为5V~5.2V,怀疑比较接近ADXL1001的输入电压上限5.25V导致传感器不工作

    3、传感器故障

    现向大神请教,敬盼回复

  • Replacing one ADXL1002 with one ADXL1001 in ADcmXL3021

    Hi

    We are interested in using the ADcmXL3021 for condition monitoring. Unfortunately, we need a range of +/- 100 g on the z-axis.

    Will there be a model which will use the ADXL1001?
    Or is it possible to easily replace the z-axis ADXL1002 with an ADXL1001…

  • 关于ADXL1001的连线问题

    想问下6个引脚怎么连接啊,同时想让评估版实时输出加速度值

  • RE: “芯”来乍到,求赞、求围观!

    捌号芯品:高频率、低噪声MEMS加速度计ADXL1001和ADXL1002

    ADXL1001和ADXL1002专门针对工业条件监测应用而设计,利用它们可实现高分辨率振动测量,为早期发现轴承故障和机器故障的其他常见原因提供必要的信息。

    过去,可用高频MEMS加速度计的噪声性能不及传统技术,阻碍了其应用,使得MEMS的可靠性、高质量和可重复性得不到发挥。

    如今,ADXL1001和ADXL1002在高频率范围的噪声性能与现有压电传感器技术不相上下,故ADI MEMS加速度计是新型条件监测产品的极具吸引力的选择…

  • RE: THe ADXL193 and ADXL278 are going obsolete what is their replacement parts and when will it be available?

    Thank you for using these products in your work and for your post!  Unfortunately, we do not have direct replacements for these devices but are releasing a number of accelerometers that might be worth your consideration.  To start with, you might want to…

  • RE: Identification of the correct G value of accelerometer

    The ADXL356 (triaxial) and ADXL1001/2 (wider bandwidth) provide a couple of options to consider. Hope this helps!

  • RE: Is it possible to change the accelerometer on CN0532? If so, what is required to do this?

    Yes, it is possible to swap ADXL1002 with ADXL1001 without any modifications to the low pass filter components.

    For other sensors in the ADXL100x family, the 3dB bandwidths are significantly different to ADXL1002 so passives will need to be modified to…

  • RE: Sensitivity of the ADXL 1000 family to infrared light

    Hi audio@audiochiemgau.de

    Thank you for your use of ADXL1001. We will investigate this further and will get back to you as soon that we have a conclusion. 

    Best Regards,
    John

  • RE: ADXL372 Noise

    Another option to consider is the ADXL1001 or ADXL1002.  These support the bandwidth you are looking for, lower noise and power than the ADXL001.  Take a look at the datasheets online.

    Anthony

  • RE: ADXL1002BCPZ

    Hi Suzuki-san (FormerMember), 

    I'm very sorry for the late reply. What we can provide you is the link to the breakout board files for ADXL1002 (ADXL1001 and ADXL1002 Breakout Board documentation: [Analog Devices Wiki] ) 

    Warm Regards, 

    JP