• adxc1501

    ADXC1501

    Dear AD, I bought adxc1501 sensors via Mouser, but without a proper datasheet, only a 1 pager, that is basically useless for configuring the sensor.

    Could you please send me a datasheet with register table to be able to use it?

    waiting for…

  • ADXC1501

    Hello AD,

    I got an ADXC1501 from DigiKey, but they couldn't provide a datasheet with pinout and SPI commands.

    Could you provide me with that?

    Thank you,

    Gabor

  • ADXC1501 - Wafer Fabrication Data

    I am looking for the FIT rate of ADCX1501 MCM. I found the Wafer Fabrication data of that MCM, but I don't know how to calculate the overall FIT value of that product. Could you please help me? Or provide some example?

  • RE: ADIS16365 accelerometer null bias issue

    Hi Mark,

    ADIS16365 sample rate SMPL_PRD is default 0x0001 meaning 819.2Hz. internal filter SENS_AVG is default setting 0x0402 meaning tap is 4. with the setting looks final sample rate is 0.1x819.2Hz=81.92Hz, is it right?

    supposed changing SENS_AVG…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • RE: 工程师的“奥斯卡”开评,大奖邀你当评委

    • “超越一切可能”最佳合作奖

    6ADI与和Dell EMC发布了一种物联网(IoT)解决方案的概念验证(POC),该解决方案可用于跟踪急救人员的健康和位置。该概念验证物联网解决方案采用了Dell Technologies与Vodafone和科克理工学院联合开发的INFINITE测试床,旨在工业物联网领域内实现创新、提供洞察力和创造商机,其应用范围覆盖众多行业。

    推荐阅读技术文章《面向急救人员的传感器融合式精密定位和跟踪方法》:http://www.analog.com/media…

  • RE: 360°全方位的ADI汽车电子技术是怎样炼成滴?围观抢百元京东卡

    (1)BMS系统。

    ADI 有完整的 BMS 系统(双精密 ADC 和精密基准电压源、ARM 处理器、闪存和收发器)集成到一个市场主导型系统级封装 (SiP) 中,树立了 12V 停止-启动 BMS 的行业标准。主要芯片有AD7284,ADUC7039等。

    (2)磁力轴位置传感器。

    ADI 的 AMR 磁力轴位置传感器提供实现这些目标所需的精度、快速响应能力和稳固性。主要芯片有AD2S1205,ADA4571等。

    (3)电流检测放大器。

    ADI 的电流检测放大器具有出色的性能,适用于各种汽车和电源管理应用…

  • 慕尼黑电子展,ADI秀最新电表技术、4D传感器与智慧城市

    2016 慕尼黑(德国)电子展已经落下帷幕,但是大家对展会上的各项技术和演示的谈论还未停止,版主也是非常开心可以和你们分享展会现场,ADI展台上的部分技术和演示。

    先来一张图看看我们热闹的展位吧~经典的黑白色,让咱们的展台看来是那么的“简洁、大气、有内涵”。

    电能/计量演示区

    ADI电表部门产品市场经理John Pitus介绍了一种新技术——mSureTm技术。这是ADI开发的一种在电表中使用的全新监控技术,能够为现场仪表提供实时精度监测,同时改进对篡改和仪表故障的检测。据John Pitus透露…