• EVAL-ADV8003-SMZ-P availability

    Dear Sirs 

    I'm searching for the following eval 

    EVAL-ADV8003-SMZ-P

    but ADI distributor in Italy has availability in 12 weeks.

    Can anyone suggest how to buy it in a time that is shorter than 12 weeks or has anyone an eval to sell me as soon as possible…

  • EVAL-Board ADV8003-p FPGA programming

    Hi,

    I need to do the routing of signal on EVAL-ADV8003-P board. to do this I need to programm the FPGA with a custom code. I see that the Boot SPI of FPGA is connected also to the processor. so, It is possible to upload a new FPGA bin file into the SPI…

  • ADV8003 configuration at start up

    Hi,

    I have a question about ADV8003 configuration.

    I see that we need to use AVES3 software to configure the device on eval board and this is fine, but in our custom board it is possible use SPI flash or I2C EEPROM for Initialize the device at the start…

  • ADV8003 RGB output sync on green

    Hi,

    I see that is possible with the ADV8003 have an analog RGB output but I don't understand if is possible have the sync signal on green or not. I need to convert a XGA signal into 576i signal with sync on green. it is possible or I need another device…

  • DDR2 loopback test on ADV8003 Eval Board

    Hi,

    I am tring to make a loopback test with ADV8003 eval board and I used these commands:

    0x1A, 0x1A5B, 0x32, // ; DDR2 change the SDRAM to be 1Gb

    0x1A, 0x1A5C, 0x25, // ; DDR2 change word size to 32 (try also with default value but same problem)

        0x1A…

  • How can i make a binary file for application EVAL-ADV8003-SMZ-P?

    I have a EVAL-ADV8005-SMZ-P. A binary sample with ADV8003-OSD-Demo work fine.
    After the i maked a build with other sample of the AnimEffect_Demo project and received a ddr2_dump.bin
    and other .c and .h files succesfull i don't understood how can i make…

  • RE: AD9984A+ADV8003

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADV8003 scripts

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADV8003 OSD

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADV8003 sync

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,