ADV7850
Attached and linked are files supporting the development of systems using the ADV7850.
If you download and use these documents, we recommend that you subscribe to notifications for post by selecting your preferred option from the Actions - Follow menu…
The user can reposition the synchronization signal output from the regenerated input synchronization signal within the CP block with the control bits as below:
• start_hs[9:0]
• end_hs[9:0]
• start_vs[3:0]
• end_vs[3:0]
• start_fe…
Hi,
I'm struggling with the ADV7850 in AutoGraphics mode when dealing with VGA non-VESA resolutions. I want to use sample data so that ADV7850 can support more resolutions.
ps: I don’t have an evaluation board.
Does anyone have code that calculates…
I am about to start a composite and s-video signal digitization project. Before i get started i need to establish which of your chips to use. I may as well start with what ever your current chip is as I may have been reading old internet webpages.
I have…
Hello
Could ADV7850 support Multi-input image segmentation or Picture-in-picture? And how much size of external DDR? Thank you.
BR
Patrick
Hi,
I have an issue about ADV7850, symptom as described below:
Now we utilize ADV7850 to develop a ADC to HDMI Box (VGA, YPbPr, S-Vide0, CVBS input), and we have designed our board and follow our distributor to fill the register but we can't display…
Hi,
This is Michael from DIVA and now we utilize ADV7850 to develop a ADC to HDMI Box (VGA, YPbPr, S-Vide0, CVBS input), and we have designed our board and follow our distributer to fill the register but we can't display our image correctly. Phenomenon…
Hey all, I am looking to use the ADV7850 for a project that involves converting the RGB signals from a JAMMA arcade board to HDMI.
1) if I am only using the CP video processor, do I need to add the DDR2 ram to the ADV7850?
2) does the ADV7850 do any kind…