• ADV7627 Design Support Files

    The ADV7627 is a 5-input, 1-output HDMI transceiver with character- and icon-based OSD.

    Product Support Item Description
    ADV7627 Product Page Link to Product Page on Analog.com
    ADV7627 Datasheet Link to ADV7627 datasheet
    SCRIPT
    ADV7625…
  • Customer hardware validation scripts for ADV7627

    We provide the attached scripts in order to assist customers with validating their hardware (boards) based on the ADV7627.

    For customer product software, we recommend that customers license the source code for our ADV7627 software driver.

    TBD

  • ADV7625 ADV7626 ADV7627 evaluation board software package documents

    Documents for ADV7625 evaluation board software package

    Advantiv_SW_Architecture_Specifications_Pr2.2.pdf Advantiv_SW_Architecture_Specifications
  • ADV7627 MCLK Frequency setting problem.

    Dear Sir :

    There were some problems with the MCLK output when we used the ADV7627 to design.

    Description 1. When the HDMI IN and the HDMI output connected.

                           The state is 1 (locked) of AUDO_PLL_LOCKED.==>And the MCLK measurement is 6.144MHz.…

  • RE: ADV7627

    Hi,

    The ADV7625, ADV7626 and ADV7627 are same functionality but only differ with cross point feature(MUX).
    ADV7627--Mux 5:1
    ADV7626--cross point Mux 2:2
    ADV7625--cross point Mux 5:2

    The ADV7627 is a subset of the ADV7625 and we use the ADV7625 manuals…

  • Is ADV7627 TX_HPD_ARC- pin a 3V logic or 5V logic?

    Hi, 

    I am having an issue with ADV7627 on my board to assert TX_HPD_ARC- when the board is connected to some monitors.  

    I measured on good monitors TX_HPD_ARC- is above 4.5V, but the failing monitors seem to show less than 4.3V.  

    If I repeatedly re-initialize…

  • RE: ADV7627 EDID

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADV7627 audio question

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADV7627 Audio Sampling rate.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,