• ADV7623 Design Support Files

    The ADV7623 is a 4-input, 1-output HDMI transceiver which supports XpressviewTm fast switching and a character- and icon-based OSD.

    This page contains the key support documents and configuration settings that a user of the ADV7623 requires; these are attached…

  • adv7623

    ADI您好

    我想设计一款HDMI自动检测装置,4路HDMI输入,1路HDMI输出,可实现HDMI输入码流的自动检测,当第一路输入无码流时自动切换至输出第2路,以此类推,请问贵司是否有成型解决方案可以推荐,如有可否申请DEMO板,谢谢!

  • ADV7623 no documentation OSD

    Hello.

    On the ADV7623 Design Support Files page, a broken link to two OSD documentation files

    ADV7623_OSD_Software_Programmer's_Guide_PrD.pdf

    ADV7623_Character-Based_OSD_Tool_User_Guide_Rev._0.10.pdf

    Where can I download these files or in what way…

  • ADV7623 support 4K/30p 4:2:2 ?

    Hi

    I want to know ADV7623 Support Video Format.

    ADV7623 support 4K/30p 4:2:2?

    ADV7623 TDMS Frequency:225MHz.

    So,I think ADV7623 support 4K/30p 4:2:2.

    Did anyone use 4K/30p 4:2:2 at ADV7623 Eva Board? 

    Best Regards.

    Take

  • ADV7623 get Multiple VSI(Vendor Specific InfoFrame)?

    Hi

    I want to know ADV7623 function.

    ADV7623 get Multiple VSI(Vendor Specific InfoFrame)?

    Some HDMI Source send some VSI(Vendor Specific InfoFrame) in 1 Frame.

    I want to get some VSI.

    ANALOG DEVICES product:ADV7610 gets Multiple VSI.

    Best Regard/

    Ta…

  • ADV7623 PIP function

    Good Day,

            Does ADV7623 have PIP (picture in picture) output function? If not, do we have new solution with PIP? 

  • RE: ADV7623

    This question has been closed by the EZ team and is assumed answered.
  • RE: ADV7623 no documents

    This question has been closed by the EZ team and is assumed answered.
  • RE: ADV7623 TX Not Powering-up

    Hi ChrisO

    Did you find a solution? we are using ADV8005 which has the same symptom  like your: even hpd_state and rx_sense_state is set, I could not power on hdmi tx by writing 1 to system_pd.

    Thanks