Hello,
I'm trying to understand what "ADI Required Write" is in the ADV7619-VER.1.9c.txt script file and where to find the definition of it's corresponding address.
What does ADI Required Write mean? Is it required?
For the 68 C0 03 ;…
Hi all.
I confirm the update of ADV7619 SWM.And I found that there are multiple difference between HUG and SWM.
#1 Page 86 HDMI map 0x48[0] RNG_OSC_PDN This bit is not describe in HUG.When will HUG update this description?
#2 Page 89 HDMI map 0x73…
Hi,
For input video resolutions with a pixel clock of greater than170 MHz, the CP core of ADV7619 is bypassed and the clock divider and the double wide (48-bit) output interface are employed.
Please let me know, Have you followed the required recommended…
Evaluation board software cannot be downloaded from the "Advantiv EVAL-ADV7619-7511 Video Evaluation Board" support file page.
Link to download evaluation board software package.sdk.analog.com/.../sdks.aspx
The dialog box does not appear at…
I have couple more questions on ADV7619:
(1) Does the chip defaults to 4:4:4 RGB mode?
(2) If there is any automatic resolution change, while using the chip, any rough estimate of how much software overhead it requires?
Thanking you in advance.
做为HDMI的接收端口,都要给HDMI发送端提供EDID信息,用于向HDMI发送端表明接收端可以接收哪种格式和分辨率的HDMI信号。
在以前的设计中,EDID信息都是存储在接收端的一块EEPROM芯片中。我看到ADV7619的FEATURE中提到支持内部的EDID,并且从UG237文档中看到ADV7619内部确实有一块RAM用于存储EDID信息。
我的问题是,有了这块内部的EDID存储区,是否就可以省去原来设计中的EEPROM芯片?虽然ADV7619掉电后,这片RAM中的EDID信息会丢失…
Hi everyone
I have a problem about use ADV7619.
I want to ADV7619 out 16 bit SDR 4:2:2 interleaved mode 0 when input 2048x1536@60 signal
My config as following:
//Vps_adv7619I2cWrite8_xxxxx(pObj, regaddr, regval);
//Init other Map Register Addr
Our customer is having questions for ADV7619. They have some monitors that can use RXA_5V. And some of the monitors they are using can not use RXA_5V. However, they have to use both monitors when HDMI cable connect to the monitors. Therefore, they propose the…
in the ADV7619 HW manual there is a bit called DATA_BLANK_EN which is not referenced anywhere else in the document. As well there is a bit called AV_BLANK_EN on figures 44 and 45. are these bits the same?
Also if i clear the bit DATA_BLANK_EN…