• ADV7613 Does ADV7613 can support Ouput 1920x720?

    Hi All,

    One of my customer is considering to use ADV7613 for his new product.

    In his application, need driver LVDS 1920x720 (Ratio 8:3) Panel , is adv7613 can output that resolution?

    HDMI Input 1920x720

    LVDS output 1920x720

    Best regards.

    Rick

  • (ADV7613)Use ADV7613 without HDCP and DDC and Audio.

    Hi !

    It is the same person as this person with ID(donadona999s).

     

    Something is wrong with my login information so I made another ID with my other mail address.

    Sorry to confuse you.

     

    I already asked about difference between ADV7613 and…

  • ADV7613 - LVDS Output ports

    Hello,

    I'm missing some information in the ADV7613 device datasheet. Can I please get my questions answered?

    I'm expecting that one clock output could be used to capture data signals of both LVDS ports, but it may be theoretically a bit more complicated…

  • We have ADV7613 in one of our hardware. Do you have the sample linux driver for ADV7613 chip.

    We have ADV7613 in one of our hardware. Do you have the sample linux driver for ADV7613 chip. If so could you share.

  • ADV7613

    I have what appears to be data misalignment wrt clock on LVDS outputs for 3 different LCD types using the ADV7613. The LCD resolutions are 1980x1080@60, 1280x1024@60 and 1024x600@60. The symptoms are pixel misalignment and misinterpretation of colour…
  • We have ADV7613 in one of our hardware. Do you have the sample linux driver for ADV7613 chip.Could you share the driver

    We have ADV7613 in one of our hardware. Do you have the sample linux driver for ADV7613 chip.Could you share the driver to me

  • ADV748X vs. ADV7613

    Hi, 

    I have a few questions regarding the ADV748X and ADV7613. I have attached the specs and block diagram flow for references of my customer's project.

    It is a HDMI to LCD application involving scaler and some drivers.

    1. I can't seem to get the…

  • ADV7613 on ubuntu

    Hello. I've an issue with adv7613.

    First of all, I have an arm ubuntu (tiny4412 SoC) with adv7613. Have no evaboard, so I've tried to configure adv7613 with  "01-01 HDMI Input_LVDS Output Port A" script from ADV7613-VER.1.1c.txt (other sections…

  • ADV7613 1080i

    Hello

    Does ADV7613 accept 1080i input and output oLDI format and let me know the technical background if not?

    As far as I checked docs, there is no description like conventional HDMI Rx ADV7611/7612/748x.

    Assumed used case is to place the ADV7613 in front…

  • ADV7613, how to configure?

    Hello, I wanna to use the ADV7613 on a self made board but I didn't found how i send the configuration that i need in my display to the chip. I have to use the XRC to configure? how i connect the ADV7613 to XRC to the program recognize it? Anyone can…