adv7611
Hi,
Cable connection can be monitor with the CABLE_DET (Using CABLE_DET_A_RAW register, we can know the raw status of port A +5v cable detection interrupt register) or even the TMDS_LOCKED register. Both of these can be mapped to an interrupt pin.
RXA_5V…
Attached and linked are several files supporting the development of systems using the ADV7611.
If you download and use these documents, we recommend that you subscribe to notifications for this post by selecting your preferred option from the Actions…
We provide the attached scripts in order to assist customers with validating their hardware (boards) based on the ADV7611.
For customer product software, we recommend that customers license the source code for our ADV7611 software driver.
TBD
The ADV7610 and ADV7611 products are very similar in functionality but they come in very different packages:
* The ADV7611 comes in a 64-Lead Low Profile Quad Flat Package (LQFP_EP) with an exposed pad in the center of the package for Ground.
* The ADV7610…
Few things often forgotten during reviews of ADV7611, ADV7612., ADV7619 and other schematics;
First - It is suggested to follow recommendation from Design Support Files pages:
For 7612: http://ez.analog.com/docs/DOC-1751
http://ez.analog.com/servlet…
Hi, i need some help at the ADV7611 chip.
I want to use this chip to convert my HDMI signal to RGB888, are there any working circuits for this used case?
I could save a lot of time.
Thanks
Hi, I want to use the ADV7611 for my Touchpanel called (Hyperpixel 4.0-Touch).
The Panel needs RGB666 and has VSYNC,HSYNC and Pixelclock and the resolution is 800x480px with 60 frames per second.
My goal is, to connect my Raspberry Pi over HDMI to the…
Original Question: CVDD's bypass capacitor of ADV7611. by Tamu
Hi,
I have some questions about your recommendation of CVDD's bypass capacitor of ADV7611.
Please refer attached file "Questions CVDD bypass capacitor of ADV7611.xlsx".
Thank…
Hi,
I have a question regrading ADV7611/19 chips. I have a device which does alter the input tmds clock to adv7611/19 , when is trying to genlock. Sometimes I am getting image shifting during the genlock process. I noticed that during initial steps of…