• ADV7524A Evaluation Board

    Hello,

     

    I am DFAE at Phoenix technologies in Israel

     

    I can’t find the EVAL BOARD DATA for ADV7524A online.

    I would greatly appreciate if you could send all necessary technical  info and part number  about EVAL BOARD for ADV7524A.

    Thanks a lot,

    M…

  • RE: HDMI芯片选型

    可以看一下ADV7511W  ADV7513  ADV7524A

  • ADV7511 vs ADV7524A

    Hello

    My customer needs an HDMI Transmitter.

    The input signal to the HDMI transmitter comes from a camera via their own ASIC which  provides a digital data bus (16,24 bits) with sync and DE signals to the HDMI chip.

    What best can be proposed for such…

  • Question about the ADV7524A

    Hi,

    I tried the support email, but I got sent here.

    Is there any documentation for the ADV7524A?
    ..from what I understand it was under some NDA, is that still the case?
    (it seems to be fairly new as there's no places stocking it yet)

    I'm doing a…

  • ADV7524A recommend register setting

    Hi ADI Expert, 

    I would like to have ADV7524A register script file or recommend register setting file, Could you help?

    Best regards.

    Ray.

  • RE: ADV7524A and ADV739X longevity

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Can ADV7524A support RGB imager input without DDR?

    Hi Scott,

    Unfortunately, ADV7524A is still under NDA (all the portable TXs are) so we can't discuss it on the forum.  You'll need to contact ADI Sales.

    Dave

  • RE: We need help to select HDMI transmitter with 24-bit RGB TTL input. We also need information about the availability, popularity, longevity, and pricing about the available parts that we will consider.

    How about the ADV7524A? Seems like it is a simpler and lower cost part, even with 16-bit only interface, it may be a good fit for us. Is it also popular and with good longevity expectation?

  • I2C speed of AD9389B/9889B

    Hello.

    I downloaded the attached file from this EngineerZone site.

    According to this, I2C speed of AD9389B/9889B is up to 100kHz.

    From page.5

    >All earlier Tx only support up to 100kHz I2C

    >AD9x89, AD9387, ADV7510, ADV7520, ADV7521
  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…