• (ADV7511W)Do you have a specification of minimum input video clock frequency?

    Hi !

    I have a question about ADV7511W.

    Our customer are using ADV7511W for R&D.

    At table 4 the specification is about only Maximum Input Clock frequency.

    Q1)

    Do you have a minimum Input Clock frequency specification ?

    Q2)

    If you don't have…

  • ADV7511W I2C Pin

    Hello

    Is it acceptable for ADV7511W to fed 1.8/3.3V through pull up register(2k) during no VDD fed to the ADV7511W? 

    Regards,

    Tomoto

  • RE: Regarding HDMI TRANSMITTER ADV7511W

    Both schemes will work.  The key is to provide clean power to the device.  I'd follow the ADV7511W reference schematic and hardware guide since it is a proven design with the ADV7511W

  • RE: ADV7511 - DVI configuration

    Hi,

    DVI Mode -  0xAF[1]
    RGB  Input   -      0x15[3:0]****0000 - 24bit RGB
                               0x15[3:0]****0101 - 12,15,16 bit RGB

    Hsync/Vsync Polarity Passthrough:


    Please refer ADV7511W Programming Guide at https://ez.analog.com/video/w/documents/779/adv7511w-design-support…

  • RE: ADV7511W Output with blank colour

    Hi,

    The ADV7511 and ADV7511W are the same die, just different pin outs.  The software should be the same except the ADV7511W has a reduced set of options that will work.

    Thanks,

    Poornima

  • RE: Parallel DVP to HDMI with ADV7511W

    Despite we would use the ADV7511W, is the EVAL-ADV7612-7511 board suitable for testing our application? 

    As I can see, the main differences (ADV7511W - ADV7511) are the width of the input pixel bus and the frequency. 

  • RE: Differences between ADV7511W and ADV7513?

    Hi Mike,

    ADV7511W is just the automotive-qualified version of ADV7513. They are otherwise the same. Unless you need the temp range and certifications for automotive, you'd be paying extra for ADV7511W for nothing.

    Dave

  • RE: ADV7511 Data sheet

    Hi,

     The ADV7511 and ADV7511W are the same, just one is rated for automotive and the other isn't. 

     So i beleive you can refer ADV7511W Design Support Files 

    Thanks,

    Poornima

  • Is ADV7511W compatible with the input signal of progressive BT.656?

    Hello,

    I have a question about ADV7511W.

    Is ADV7511W compatible with the input signal of progressive BT.656?
    If it's supported, could you tell me the register settings for this?

    Thank you.
    Best regards.

  • Comment on ADV7511W Design Support Files

    Hi

    Just noticed a typo on "ADV7511W_Hardware_Users_Guide.pdf Rev.A"

    Table 3 Complete Pinout List ADV7511W

    HPD is assigne on 30pin but actual is 16pin(like ADV7511W datasheet).

    30Pin is CEC.

    Regards,

    Tomoto