• ADV7510 HDCP error

    I'm bringing up the ADV7510 on a custom PCB. I'm able to receive EDID data. My ISR is clearing VSYNC interrupts. No video yet.

    When I enabled HDCP, register 0xC8 is reporting b0100 0011.

    Which translates to:

    HDCP State: 0011 - Initializing…

  • Using ADV7510

    ************************************************************************

    Content in this post contained proprietary information that was removed by an ADI moderator. 
    Please consult the EngineerZone Code of Conduct for posting guidelines.

    ********…

  • HDCP with ADV7510

    Hello,

    we use the ADV7510 as transmitter. Is there a possibility to check wether a connected Rx supports HDCP without initiating the hdcp handshake sequence?

    Thanks.

  • ADV7510 Design Support Files

    Attached and linked are files supporting the development of systems using the ADV7510 HDMI Transmitter.

    We recommend that, if you download and use this document, you subscribe to email notifications for either the entire forum or at least this FAQ…

  • adv7510 RGB quantization range

    can anyone explain how RGB qunatization range control bits work in adv7510?

    according to adv7510 programming guide, addr 0x57 bits[3:2] control RGB quantization range, it can be set to enable either limited range or full range, with flat RGB input I…

  • RE: ADV7510 HDMI questions

    I'm reading Chip Revision = 0x02 on my ADV7510 evaluation board, so I suspect the ADV7510 Programming Guide (rev D) is incorrect.

    So I assume the Gennum IC does not have HS, VS, or DE. Is that correct? In that case, you will need to configure the…

  • ADV7612 ADV7510 Handshake Failure

    Hello everyone,

    I am using the ADV7612 on the receiver side, when I connect it to a device (through hdmi cable) using the ADV7510 I do not see any communication happening on the DDCA lines between the two devices.  I have DDCB disabled on the receiver…

  • adv7510 input video format

    Hi,

    adv7510 supports several input video formats, one mode that we want to use but missing is 24bit RGB4:4:4 or YCbCr4:4:4 with embedded sync, can adv7510 support such input video format? how?

    BTW I have used 24bit RGB4:4:4 and YCbCr4:4:4 with separate…

  • ADV7510 - 480i, 576i

    I am trying to get output resolutions 480i and 576i through DVI/HDMI on this devices but the video is shaky and cuts out.  We are sending the data to the chip right out of the CEA-861 spec VIC 7 and Vic 22.  Is there some errata for 480i/576i?7 and VIC…

  • Ri Mismatch with ADV7510

    We are developing a HDCP repeater device with ADV7441 as receiver and ADV7510 as transmitter.

    We have implemented the repeater software and are now testing with different video sources and displays.

    All works fine so far, except for two displays: