• ADV7482 Antialiasing Filters setting

    Hi,

    I have a question about ADV7482 antialiasing filters setting.

    1) If "aa_filt_man_ovr" and "aa_filt_en" are default, are the registers selected by "insel" enable?
    2) Should we set "aa_filt_man_ovr" to 1(Enable override…

  • ADV7482 I2S output

    Hi

    My customer would like to use I2S output data from HDMI source when operating MIPI Tx A port sourced from CVBS input.

    is it possible?

    if yes, could you provide sample register script file to me?

  • Freeze gain of ADV7482

    Hi,

    I would like to know the setting (Freeze gain) of LAGC [2:0] = b'111.
    After automatically adjusting the gain with AGC [2: 0] = b'010 etc., is it possible to fix the gain value in that state by setting LAGC [2:0] = b'111 (Freeze gain)?

  • ADV7482 HDMI _ DVI detection

    Hi
    We found that HDMI input to ADV7482, then ADV7482 detection is DVI mode. 

    What is situation will case detection is incorrect? 

    need to check registers setting or circuit of ADV7482? 

    Thanks.

  • About "range" register of ADV7482

    Hi,

    I have a question about "range" register of ADV7482 and please see the attached file for details.

    * Q1
    I'd like to know how to handle data over Y236/CbCr240 or below Y16/CbCr16) when the "range" register is set to "0".…

  • RE: [ADV7482] How to use CP_BRIGHTNESS[7:0] in RGB output mode?

    Hi,

    My understanding is it is impossible to adjust offset for NEGATIVE with a4, b4 and c4.

    is this right?

       When referring the hardware manual it seems(Page 188), the coefficients can only be programmed in the range [-0.99 … +0.99] - Range is between positive…

  • (ADV7482)Does ADV7482 has flash memory or DRAM?

    Hi 

    Does ADV7482 has flash memory or DRAM?

    Best regards

    Kawa

  • (ADV7182A and ADV7482) Unused analog input

    Hi 

    I have a question about ADV7182A and ADV7482A.

    At these thread, ADI answered to connect unused AIN to GND.

    https://ez.analog.com/video/f/q-a/9918/adv7181d-unused-pins

    https://ez.analog.com/video/f/q-a/12611/adv7180-unused-inputs-unused-xtal-pins

    https…

  • ADV7482 update speed for the peak white algorithm by LAGT

    Hi,

    I would like to know the update speed for the peak white algorithm by LAGT when I set lagc[2:0]=010 (default) and lagt[1:0]=11(default).
    *In the Hardware Manual, it is described "Adaptive" but please let me know the reference value.

    Could…

  • (ADV7482)EDID

    Hi

    I have a question about ADV7482 EDID.

    ADV7482 hardware manual "ADV748x_HardwareManual_RevPrB_2014-07-11_1.pdf" "5.3.1.4 EDID Controller" has the following description.
    --------------------------
    The E-EDID/repeater controller is reset…