Hello,
Can someone explain what actually happens to Vsync Out of ADV7403 when the FR_LL[10:0] is changed?
Kindly guide me.
Thanks
Hi I am currently working with ADV7403 how can it be used to add subtitles into a PAL based video
Good day!
We use ADV7403 decoder in our design. If we set 30-bit @ LLC2 4:4:4 mode in output control register(offset 0x03) then there is no data (zero data) on any outputs. We don't change any default values in the decoder registers. CVBS in on…
Regard ADV7403
Input Config: Analog RGB form PC-Computer connected to ADV7403 on AIN1-Green AIN2 Blue AIN-3 Red Vsync to VS-IN, Hsync to HS_IN (All Other exactly as the EVB Schem)
Config Prime Mode 010b GR VID_STD 1100b for 1024x768 _@ 60 (Exactlly…
Hello
We are using the ADV7403 in the PAL mode (SDP). Some days ago I saw a strange problem - when I try to switch between two video channels, sometimes the IC is unable to lock the video and I see complete garbage on the screen (mostly white lines and…
hello,
Did ADV7403 do any 1080p format testing? Could ADV7403 support YPBPR 1080P component input?
rita whrite
Hi
I have few questions regarding ADV7181C, ADV7403 and similar products
1. Is there any way to use the ADV7181C for SXGA resolution. (I prefer using this device because it is small package device)
2. According to the data sheetThe ADV7403-140 can…
Hi,
I downladed "ADV_Register_Control_Ver_7.0_Installation_ADV7403.zip" from ftp.analog.com:/users/decoders/ADV7403/Software .
Then I tried to unzip it by 7-zip,but it failed because of header error.
Please let me kow how to fix this.
( 7-zip…
I'm trying to get color framing from ADV7403.
Input Signal : NTSC
Device : ADV7403
Registers :
ADDR(0x00) = 0x00
ADDR(0x03) = 0x10
ADDR(0x04) = 0x47
ADDR(0x05) = 0x00
ADDR(0x06) = 0x02
ADDR(0x07) = 0x2F
ADDR(0x15) = …
Hi There ,
I am trying to make ADV7403 video decoder to output 10-bit data from analog input of a PAL camera .
FPV Camera data sheet says its PAL output is in two formats 1020Hx596V and 976Hx582V , my task is to configure ADV7403 to output stream in BT…