• Regarding alternatives to ADV7393.

    Good day.

    Could you please tell me the successor or alternative to ADV7393?

    I checked your website and found that ADV7393 is deprecated for new design.

    I am looking for a successor or replacement to ADV7393.

  • Supplying power to EVAL-ADV7393 from a ZCU102 (over FMC)

    I have the EVAL-ADV7393 eval board, and I need to provide the inputs to the EVAL-ADV7393 from a Xilinx ZCU102 development board via 1 of the 2 HPC FMC connectors.  The inputs to the EVAL-ADV7393 eval board are provided over P1, whose pinout is shown below…

  • ADA4891-1W schematic review at ADV7393 DAC output

    ADA4891-1W schematic review at ADV7393 DAC output by Steven.yang@analog.com

    Hi

    As we discussed, customer would like to apply video buffer amp for 720p YPbPr at ADV7393 output.

    I draw the schematic and the configuration as well in attached file.

    ADA4891…

  • [#5698] rtc wake up from standby mode fails on bf537 with adv7393 installed

    [#5698] rtc wake up from standby mode fails on bf537 with adv7393 installed

    Submitted By: Vivi Li

    Open Date

    2009-11-18 04:41:40     Close Date

    2009-11-27 03:32:08

    Priority:

    Medium     Assignee:

    Michael Hennerich

    Status:

    Closed     Fixed In Release:

    2010R1

    Found In…

  • FAQ: [#5977] adv7393 power test failed in both standby and mem mode(2010)

    [#5977] adv7393 power test failed in both standby and mem mode

    Submitted By: Vivi Li

    Open Date

    2010-03-18 05:03:03     Close Date

    2010-03-22 00:33:18

    Priority:

    Medium     Assignee:

    Michael Hennerich

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release:

    2010…

  • RE: Thank you! Please consult aves blue.ADV7180+ADV7393 i2c?

    In theory you can create a DLL for any I2C interface as long as you follow the interface specifications.  However to fully test and debug it you would need to work with the source code.  We cannot release the source to the public. It can only be accessed…

  • ADV7393 Camera Module Interface

    Hello,

    I am trying to get an ADV7393 to interface with a monochrome camera. The camera output is 320x240@60fps with 8-bit parallel data bus, hsync and vsync. I would like the ADV to output NTSC video at 240p, preferably with square pixels, non-interlaced…

  • FAQ:[#6326] Wakeup from mem has error with adv7393/tftlcd on bf537-stamp in 10r1 branch(2010)

    [#6326] Wakeup from mem has error with adv7393/tftlcd on bf537-stamp in 10r1 branch

    Submitted By: Vivi Li

    Open Date

    2010-11-01 07:24:03    

    Priority:

    Medium     Assignee:

    steven miao

    Status:

    Open     Fixed In Release:

    N/A

    Found In Release:

    2011R1     Release:

    Category…

  • DOES ADV7393 SUPPORTS RS-170 ?

    Hello,

    I'm working on a project where I need to support both video formats:

    1. NTSC

    2. RS-170

    I can see in the ADV7393 SPEC few mentions regarding the NTSC but nothing about RS-170,

    my question is - does the ADV7393 supports RS-170 ?

    thank you,

  • ADV7393 Design concern

    We are planning to use ADV7393 chip in our design. please let me know, if this chip support 2.5V IO pins logic? or fixed 1.8V or 3.3V?

    and someone please assist us to review the attached schematic (here we used level converter )