• RE: ADV7281-M image too dark or too bright and analog noise

    Hi,

    Its seems this issue is something related to linux kernel driver

    Here you can find ADV7280 linux driver http://git.toradex.com/cgit/linux-toradex.git/tree/drivers/media/i2c/soc_camera/adv7280.c?h=toradex_tk1_l4t_r21.5

     Also there is a separate forum…

  • ADV7281/ADV7281-M / ADV7281-MA Design Support Files

    This page contains the key support documents and configuration settings that a user of the ADV7281, ADV7281-M or ADV7281-MA requires.

    The ADV7281 is an SD Video Decoder that output digital video data in an 8-bit YCrCb format over an ITU-R BT.656 link…

  • Interlaced feed on ADV7281-M

    Team,  

      We are currently facing a concern, the below s our configuration( please ignore the LVDS path)

    We are getting an interlaced feed to the infotainment , which uses a ADV7281 decoder, when we read the status register 0x13 on 7281m we get a value…

  • [ADV7281-M] Manually trigger interrupt pin INTRQ

    Hi all,

    I want to trigger the interrupt pin (INTRQ)

    I tried to achieve this by using the manual interrupt, using the following sequence for I2C address 0x42:

    1. Enter Interrupt sub map register space [Write 0x20 to Addr 0x0E]
    2. Set Interrupt configuration…
  • Does ADV7281 support merge mode?

    I am looking to replace the Epson S2D13P04 multi camera IC in a design. This part supports various video modes, one of them called 'merge mode' which resizes all 4x video inputs and formats them into one frame.We were initially looking at the ADV7281…

  • RE: ADV7281

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADV7281 clock

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADV7281 configuration

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADV7281 I2C config

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,