• replacing ADV7183

    I'm currently using an ADV7183 in my product and it is not recommended for new designs.

    I really Only need 1 composite input and to support NTSC and PAL.

    I was looking at other Video decoder chips in this list http://www.analog.com/en/analog-to…

  • ADV7183/84 ident code

    We manufacture a product using either the ADV7183 or ADV7184 and I would like to be able to distinguish between the two models via code.

      

    So far, I am aware that the IDENT register (0x11, p. 86 of the above-mentioned manual) can return 0x11 or 0x19…

  • Migrating from ADV7183 to ADV7184

    Hi,

    We're currently migrating a board from a AV7183b to an ADV7184, but I can't seem to find a specific Visual DSP++ driver for the ADV7184. Can we just use the adi_adv7183.c one? Do we need to worry about the extra registers or will the 7184 behave…

  • ADV7183 and QVGA (320*240 pixels)

    Hello,

    I have a product setup to capture VGA size images (720*480 pixels) from ADV7183 in CCIR format. My target DSP is a bf548. It is all working well and great with help of using diverse application notes and examples. My circuit is a true copy of…

  • How to process black and white image on ADV7183

    One customer is using ADV7183 and ADV7170 for processing black and white image, could you please suggest the register settings for black and wihte image?

  • [#5484] adv7183 test failed in trunk on bf561-ezkit

    [#5484] adv7183 test failed in trunk on bf561-ezkit

    Submitted By: Vivi Li

    Open Date

    2009-09-02 22:28:20     Close Date

    2009-10-13 03:57:37

    Priority:

    Medium     Assignee:

    Michael Hennerich

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release:

  • 2011-06-06 09:15:23     Old BF561EZKIT with ADV7183

    2011-06-06 09:15:23     Old BF561EZKIT with ADV7183

    Vladimir Fusek (CZECH REPUBLIC)

    Message: 101010   

    I have very old board BF561EZKIT rev. 1.3. Trying to compile kernel (2008R1.5RC3 with last toolchain). I did everything here https://docs.blackfin.uclinux…

  • Problems with video resolution on Pal mode on BF537 - adv7183

    Hi,

    I'm trying to take video images live from a panasonic video camera which works on Pal format. The problem is that the images are doubled when they are put in the Blackfin memory and I want to put them corectly in DMA.I believe I have to modify the…

  • [#5601] Remove blackfin_cam module will make kernel hang for VS6624 and adv7183

    [#5601] Remove blackfin_cam module will make kernel hang for VS6624 and adv7183

    Submitted By: Vivi Li

    Open Date

    2009-10-13 04:10:50     Close Date

    2009-10-15 03:50:26

    Priority:

    Medium     Assignee:

    Michael Hennerich

    Status:

    Closed     Fixed In Release…

  • FAQ: [#7089] fail to build adv7183 on bf561-ezkit in kernel 3.3(2012)

    [#7089] fail to build adv7183 on bf561-ezkit in kernel 3.3

    Submitted By: Vivi Li

    Open Date

    2012-04-28 05:23:09     Close Date

    2012-05-07 01:31:13

    Priority:

    Medium     Assignee:

    Scott Jiang

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release: