• ADV7128: Used for Audio application

    I need to convert as digital audio signal back to analog. I know that the
    ADV7128 is a video DAC but can it be used to convert an audio signal in the
    same manner.

     

    The ADV7128 is optimised for computer video graphics, although you can think of…

  • RE: ADV7128 artifacts in PAL

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: The acceptable voltage of negative voltage spilke with short time below -0.3V(30ns every 10us), without causing latch-up and degradation and failure for ADV7182&ADV7182A?

    The ADV7128 is not specified to operate beyond the range listed in Table 7, Absolute Maximum Ratings.  Operations and reliability outside this range is not specified.

  • ADV7182: No signal on LLC pin

    I have configured ADV7128 register via IIC and got the correct ack signal. The ADV7182 is set in free-fun mode, and output Boundary box. Register bit TRI_LLC is set to 0 (LLC pin active).

    The crystal also works properly. However, there is no signal…

  • RE: About ADI Recommended Write of ADV7182 in ADV7128CUST-VER2.6.txt

    Hello Takepiro,

    ADV7128 is an obsolete product.  Do you mean it or ADV7182?

    In either case, those writes are generally determined at characterization and we don't disclose the details except to say you must write them.


    Dave

  • RS-343 Video

    I have a customer looking to capture RS-343 video (high resolution monochrome composite video used primarily in mil/aero) and wanted to know if we have any parts that have been used to do this? I was thinking maybe the ADV7181C could do the job but am…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…