• ADV3226 Evaluation Board Design Support Files

    Hello,

    Are there design support files for the ADV3226 Evaluation Board?   I need the schematic, BOM, PCB design files, etc.  I've searched up and down on Analog's site and Engineering Zone without success.  Can you help?   Thank you!

    Dan Ngai

  • Need check series termination(IBIS Model) for ADV3226.

    Need check series termination(IBIS Model) for ADV3226.

    We have tested evaluation board of systems using ADV3226 and one port input 75ohm CATV signal
    ,but insertion loss about 5db.
    How we up on analog gain?

    We still do not know what example and guidelines…

  • RE: Can we use AD8115 as one input to multiple output video switch?

    Hi, Gautam.

    Definitely yes! You can use multiple output from a single input. Just enable all outputs to a certain input just like the GUI setting below. As you can see, ADV3226/7 GUI was used. This is because ADV3226/7 GUI is compatible with AD8115-EVALZ…

  • ADV3226_ADV3227 Design Support Files

    Attached are the evaluation board schematic, layout and software which will support the development of systems using the ADV3226 and ADV3227.



  • RE: Regarding Absolute Maximum rating for ADV3228

    Hi, Gautam.

    As confirmed by the designer of the ADV3228, the absolute maximum potential difference of DVCC to AVEE is 11V. This applies to other crosspoints such as the ADV3224, ADV3225, ADV3226, ADV3227, and ADV3229. We'll update the datasheets and…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225