有没有ADV3224评估版的代码
This kit arrived with a board, a USB cable, and nothing else. Is there a User Guide or application software for running this?
For Figure 15 in the datasheet of the ADV3224, should the output voltage range be that low?
The documents and software supporting the development of systems using ADV3224, ADV3225, ADV3228 and ADV3229 can be downloaded in these links:
ADV3224_3225 Design Support Files
ADV3228_3229 Design Support Files
Hello,
I use ADV3224 in my design.
Datasheet said, that this device drives 150 Ω loads. I have a video signal, Fsig=5 MHz, scheme of my design in file, I use highpass filter C=20uF R2=5,1KΩ series with ADA4430 after ADV3224 and after through potential…
Attached are the evaluation board schematic, BoM and evaluation board software which will support the development of systems using the ADV3224 and ADV3225.
Hi, Gautam.
As confirmed by the designer of the ADV3228, the absolute maximum potential difference of DVCC to AVEE is 11V. This applies to other crosspoints such as the ADV3224, ADV3225, ADV3226, ADV3227, and ADV3229. We'll update the datasheets and…