Hi,
As per specification, "ADV3200/ADV3201 are specified with excellent differential gain and phase when driving a standard 150 Ω video load, the crosstalk will be higher than the minimum obtainable due to the high output currents"
It…
Hi,
As per specification, "ADV3200/ADV3201 are specified with excellent differential gain and phase when driving a standard 150 Ω video load, the crosstalk will be higher than the minimum obtainable due to the high output currents"
It…
Hi,
ADV3201 output is interfaced to AD725 input.
In datasheets of ADV3201 and AD725 both mentioned 75ohm shunt resistance at output and input respectively.
Whether is it required the 75ohm shunt resistance both the ends?
Regards,
Siva
Hi,
We have a video signal from 0V to 1V, is it possible to enter into ADV3201(supply at +-3V3)?
regards,
Dario
Can ADV3200 and ADV3201 DVCC be equal to 3.3VDC?
I can't find this information on the datasheet and on the eval board documentation DVCC is 5V.
Thank you for your support
Best Regards
Marco
I want to use ADV3201 to route RGB analog video . I have negative sync on analog video: my question is if I need dual supply or if sync-tip clamp feature has the option to avoid to use dual supply. More in general I don't understand how sync-tip clamp…
Hi,
Please share the detailed design support files for ADV3201, which is not available in website.
I required the reference schematic and IBIS files urgently.
Regards,
Siva
Hello,
AD8145 operates from +5V & -5V
ADV3201 operates from +3.3V & -3.3V
In case without negative supply powered on the both the IC's, What will happen the IC?
What is the maximum delay can maintain for both supplies are raise?
--Siva…
As long as the ADV7343 outputs standard CVBS signals into the nominal 75 Ohm load it should interface to the ADV3201. The ADV3201 is expecting inputs as shown in Figure 107
Hi,
Try altering the Vref of the ADV8005 or AC couple it to the input of ADV3201.
Regards,
Goz