Hi,
From datasheet of ADV3200 I see that is possible to have Multicasting, so is possible to map to two or more output ports the same input port? or this device support only a 1 to 1 connections?
regards,
Dario
Hi,
From datasheet of ADV3200 I see that is possible to have Multicasting, so is possible to map to two or more output ports the same input port? or this device support only a 1 to 1 connections?
regards,
Dario
Hi,
From datasheet of ADV3200 I see that is possible to have Multicasting, so is possible to map to two or more output ports the same input port? or this device support only a 1 to 1 connections?
regards,
Dario
Can ADV3200 and ADV3201 DVCC be equal to 3.3VDC?
I can't find this information on the datasheet and on the eval board documentation DVCC is 5V.
Thank you for your support
Best Regards
Marco
Hi,
I am using ADV3200 in one of our PCB design with supply requirement of +2.5 and -2.5V (input signal is ranging between +1.7V to -1.7V) . Few questions;
Hi,
If I use the ADV 3200 with single supply at 5V, which is the logical level for digital I/O? In datasheet I see that is present the table with the value for 3V3 digital supply but I can't find the one for 5V.
moreover, is possible use 5V to supply…
Hi,
with one rail(5v) power supply (5V on Vpos and 0 on Vneg), the bypass capacitor of VNEG (that is at GND) are no more necessary?
regards,
Dario
Hi,
As per specification, "ADV3200/ADV3201 are specified with excellent differential gain and phase when driving a standard 150 Ω video load, the crosstalk will be higher than the minimum obtainable due to the high output currents"
It…
Attached are files that would support the development of systems using the ADV3200 and ADV3201.
The software is too large (418MB) to be uploaded here. In case you need it, please email me at anna-fe.briones@analog.com or please contact your point of…
最新中文资料更新
中文数据手册
AD7150: 用于接近传感的超低功耗双通道电容式转换器
AD7980: 16位、1 MSPS PulSAR ADC,采用MSOP/QFN封装
AD8057/AD8058: 低成本、高性能电压反馈型、325 MHz放大器
最新中文资料更新
中文数据手册
AD7150: 用于接近传感的超低功耗双通道电容式转换器
AD7980: 16位、1 MSPS PulSAR ADC,采用MSOP/QFN封装
AD8057/AD8058: 低成本、高性能电压反馈型、325 MHz放大器