• ADUX1020 gesture question

    I am currently working on the project which makes use of ADUX1020 board. The board is interfaced to the ADICUP3029. I am just making use of pins of J1 (SCL, SDA, 1.8V and gnd). I have attached the screenshot of the same. I doubt whether the LED is getting…

  • ADUX1020 Driver C Code

    Hi everyone im just wondering if i can make the ADUX1020 driver c code convert to Arduino code. 

  • ADuX1020 EVB

    HI,I check UG1022(ADUX1020-EVAL-SDP manual)and it does not include main bord circuit.

    could you give me a circuit of Main bord?

  • ADUX1020 Mounting Recommendations

    Hi,

    Could sensor area of ADUX1020 be cleaned/washed by spirits or other liquids after mounting on a PCB? Do you have any recommendations?

    Regards,

    Ivan

  • RE: How can peak LED currents greater than 250 mA be used with the ADUX1020, to achieve operation at greater range?

    Hello Tylerray;

    On datasheet; it says proximity sensing to 20 cm. Can ADUX1020 support a longer range like 50cm? If yes; how to achieve it?

    Thanks;

    Bell

  • RE: ADUX1020-Eval-SDP 64 bit drivers not working at Windows 10

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • On the attachment of water to ADUX1020 Sensor

    Hi,

    I would like to use ADUX1020 in the kitchen and so on.

    Even if water is attached to the LED receiving part or a waterproof cover is attached, is it possible to perform gesture recognition normally?

    Is there no loss of accuracy due to light refraction…

  • ADUX1020 Field of View

    On the datasheet, the ADUX1020 has a 120 degree field of view. In our testing, we measured a 60 degree FoV. Can you explain if this is a typo, a mistake, or if the measured angle means something different?

  • ADux1020 gesture question

    Hi Sir,

     

    we have some question about ADux1020, could you help to check this, thanks you very much!

    1. We  found out that the rotation is very hard to recognize and we want to know that does ADI have related document to explain how to achieve or the…
  • Question for Gesture Sensor ADUX1020

    Dear Sir/Madam,

    I got the interested in your gesture sensor evalboard ADUX1020-EVAL-SDP and ADUM1020-EVALZ-LED.

    What voltage and current should we add for ADUM1020-EVALZ-LED?

    Up to 12V(AC to DC adaptor),OK?

    Your label enclosed at ADUM1020-EVALZ-LED…