• ADUX1020 10cm detection distance

    Hello

            If object is finger, could ADUX1020 meet 10cm detection distance while finger closed? Thank you. 

    BR

    Patrick

  • ADUX1020-EVAL-SDP

    Hello

     I am trying to evaluate the ADUX1020-EVAL-SDP kit on a Widows 7 after installing the Optical Gesture Evaluation Tool (Rev. 1.5.1).

    However, I am getting a pop-up of ‘No Device Found’ after File->Connect>SDPASIC Bridge (Debug).

  • RE: which led is mounted on adux1020 evaluation board?

    Hi Tyler,

    I had a project need proximity distance 300mm, seems SFH4046 is good.

    Would you please help to suggest the LEDx current and spacing between ADUX1020 and LED?

  • Scaling values for ADUX1020 proximity mode

    Hello, 

    I'm writing an IIO driver for ADUX1020 sensor and like to know the scaling values for the SAMPLEI, SAMPLEX, SAMPLEY register values in proximity mode. How can I turn these raw register values to meaningful intensity and proximity values?

  • Questions about ADUX1020 Evaluation board

    Hi there,

    I have some questions about ADUX1020 Evaluation board.

    #1, I need a reference of PCB design, please tell me where I can get the Evaluation board's PCB information.

    #2, I need to know the cover material for ADUX1020. Please tell me where…

  • ADUX1020 Field of View

    Hi,

    I would like to use ADUX1020.

    So, I have a question. Please help me.

     

    Question:

    It is stated that the ADUX1020 has a 120 degree viewing angle(data sheet).

    Please tell me about the measurement conditions at this time.
    What I want to know is the LED…

  • EVAL-ADUX1020 under Win10 functions?

    Hello,

    I downloaded the software from https://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-adux1020.html#eb-relatedsoftware

    And tried to install it (also with elevation) under Win10. 

    But I got the error 

  • ADUX1020 Data Read Error

    I am trying to interface with the ADUX1020 but I am not able to read any data values from the device.  I am able to set register 0x45 to 0x01, to enable proximity mode, and if I read back the value at this address it is 0x01.  However if I read the data registers…

  • About ADUX1020 Using

    Hi,

    I would like to use ADUX1020.

    So, I have two questions.

    #1  Are there any recommended LEDs for external LEDs?

        What kind of LED can I use?

    #2  I would like to have algorithms themselves put in microcontrollers, etc. and process them.
        Is software…