• RE: negative ground with ADuM7440

    This question has been closed by the EZ team and is assumed answered.
  • ADuM7440 芯片Latch-up时的现象是什么?

    Hello 您好:

    最近在使用贵司的ADuM7440芯片,但是在使用中遇到了一些问题,拜托帮忙解答一下,感谢!

    问题1,ADuM7440芯片手册中有写  [ Common-mode transients exceeding the absolute maximum ratings may cause latch-up or permanent damage. ]

    ,想问一下,芯片Latct-up时,芯片的输出现象是什么?

    问题2,   ADuM7440  Latch-up 后,能够恢复成正常状态吗?

    问题3…

  • ADuM7440怀疑静电损坏,如何测量单体

    基板上使用了四枚相同的ADuM7440,基板机能故障,怀疑芯片受到静电损坏,更换了其他四枚芯片后,基板机能恢复.

    如何测试单体芯片是否有问题.

  • ADuM7440怀疑静电损坏,如何测量是否损坏

    在基板上使用了4个ADuM7440,但是进行性能测定时有问题,将四个ADuM7440更换后,问题解决.

    怀疑是基板在使用时没有接地,由于静电的原因导致芯片损坏.

    但是对拆下来的芯片进行测量,两侧的二极管没有问题,请问如果想确认芯片如果受到静电损坏会有什么现象,如何能够使用芯片单体测量出来.

  • ADuM7440 EMI vs Data-rate

    Hi,

    I'm looking at using the ADuM7440 in a design that has restricted space and I will therefore have a limited ability to build stitching capacitance inside the PCB (I only have space for maybe 5pF - 30pF depending on how I change the stack-up). I have…

  • RE: ADI教你实现高分辨率、低噪声的工业电磁流量计系统!

    相关器件:

    36 V、1 A同步降压DC-DC调节器ADP2441:https://www.analog.com/cn/products/adp2441.html

    精密、微功耗、分流模式基准电压源ADR5040:https://www.analog.com/cn/products/adr5040.html

    1 kV RMS四通道数字隔离器ADUM7440:https://www.analog.com/cn/products/adum7440.html

    单通道、12位、串行输入、电流源DAC AD5410…

  • 隔离器中的CMTI指标如何评价?

    我现在在用ADuM7440型隔离器,手册里面提到了CMTI指标,需要产生一个高压高摆率的信号源,请问什么设备可以实现该信号源?能否推荐一个型号?谢谢。

  • CMTI指标测试

    你好,我现在在用ADuM7440芯片,手册里面提到了CMTI指标的测试,前期已了解到ADI是采用高压电源结合高压开关来实现这个高压高摆率的信号。我现在仍然遇到了以下问题:

    1、我没有找到DEI HV-1000-P 的相关资料,能否提供相关生产厂家或链接网址?BHK2000-0.1mg的输出电流最大为100mA,测试时如何控制才能不对芯片造成损伤?另外,高压开关与高压电源如何组合,才能形成高摆率信号?

    2、按照UL1577,隔离器的隔离电压指标在生产测试时为认证时电压的1.2倍,且在1秒内测量…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • Unpower one side on ADUM744X

    Hi,

    I was wondering if it was dangerous for the ADUM to unpower one side? All inputs on the unpowered side are connected by a pull down resistor and will not have any signal on it.

    Thanks

    Dave Lacerte